2019-01-17 8:31 PM
Hi eveyone,
I have a problem with RTC wake up. I use LSE 32.768kHz.
I run example from manufacturer to wake up MCU from Stand by mode very 1min, 2mins. Everything work okay.
But, When I put delay 10s and HAL_PWR_EnterSTANDBYMode(); into while(1). Everything is not okay.
The RTC does not wake up on time, when I delay 10s it will lack of 10s, when I delay 20s it lack of 20s. I try to do it many times.
How can I wake-up mcu on time in time I set?
Thank you for any help.
int main(void)
{
HAL_Init();
/* Configure LED3 */
BSP_LED_Init(LED3);
/* Configure the system clock to 2 MHz */
SystemClock_Config();
/* Configure the system power */
SystemPower_Config();
/* Check and handle if the system was resumed from StandBy mode */
if(__HAL_PWR_GET_FLAG(PWR_FLAG_SB) != RESET)
{
/* Clear Standby flag */
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_SB);
}
/* Disable Wakeup Counter */
HAL_RTCEx_DeactivateWakeUpTimer(&RTCHandle);
/*## Setting the Wake up time ############################################*/
/* RTC Wakeup Interrupt Generation:
Wakeup Time Base = (RTC_WAKEUPCLOCK_RTCCLK_DIV /(LSE or LSI))
Wakeup Time = Wakeup Time Base * WakeUpCounter
= (RTC_WAKEUPCLOCK_RTCCLK_DIV /(LSE or LSI)) * WakeUpCounter
==> WakeUpCounter = Wakeup Time / Wakeup Time Base
To configure the wake up timer to 4s the WakeUpCounter is set to 0x1FFF:
RTC_WAKEUPCLOCK_RTCCLK_DIV = RTCCLK_Div16 = 16
Wakeup Time Base = 16 /(~39.000KHz) = ~0,410 ms
Wakeup Time = ~4s = 0,410ms * WakeUpCounter
==> WakeUpCounter = ~4s/0,410ms = 9750 = 0x2616 */
HAL_RTCEx_SetWakeUpTimer_IT(&RTCHandle, 0x2616, RTC_WAKEUPCLOCK_RTCCLK_DIV16);
/* Insert 5 seconds delay */
HAL_Delay(5000);
/* Clear all related wakeup flags */
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU);
while (1)
{
HAL_Delay(10000);
/* Request to enter STANDBY mode (Wake Up flag is cleared in PWR_EnterSTANDBYMode function) */
HAL_PWR_EnterSTANDBYMode();
}
}
Solved! Go to Solution.
2019-01-24 2:56 AM
Hello,
Why you do not set the wake up time by setting the wake counter in the HAL_RTCEx_SetWakeUpTimer_IT function.
Instead of adding the "HAL_Delay" function, you can simply customize your wake up time like this:
- For example if you want to waking-up the MCU after 10 seconds:
You need just to calculate the value that you want to set.
Best Regards,
Mohamed Aymen.
2019-01-22 5:08 AM
Hello,
I think that you are working with an STM32L4 device ?
Why you put the HAL_PWR_EnterSTANDBYMode() in the while(1) loop ?
Best Regards,
Mohamed Aymen.
2019-01-22 10:58 PM
Hello mohamed-aymen.hzami,
I use STM32L151
I put HAL_PWR_EnterSTANDBYMode(), because I want to run my program in while(1). After that I put microcontroller into stanby mode, and it will wake up after 1min
I try to use HAL_RTC_DeInit(&hrtc); after call HAL_RTCEx_SetWakeUpTimer_IT(&hrtc, timeMin, RTC_WAKEUPCLOCK_CK_SPRE_16BITS); and before call HAL_PWR_EnterSTANDBYMode(), I call HAL_RTC_DeInit(&hrtc);
My program run and wake up on time. But In the first run, it wake-up immediately, after that it run true. I don't know why.
Below its my code. Thanks for your attention.
int main(void)
{
HAL_Init();
/* Configure LED3 */
BSP_LED_Init(LED3);
/* Configure the system clock to 2 MHz */
SystemClock_Config();
/* Configure the system power */
SystemPower_Config();
/* Check and handle if the system was resumed from StandBy mode */
if(__HAL_PWR_GET_FLAG(PWR_FLAG_SB) != RESET)
{
/* Clear Standby flag */
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_SB);
}
/* Disable Wakeup Counter */
HAL_RTCEx_DeactivateWakeUpTimer(&RTCHandle);
/*## Setting the Wake up time ############################################*/
/* RTC Wakeup Interrupt Generation:
Wakeup Time Base = (RTC_WAKEUPCLOCK_RTCCLK_DIV /(LSE or LSI))
Wakeup Time = Wakeup Time Base * WakeUpCounter
= (RTC_WAKEUPCLOCK_RTCCLK_DIV /(LSE or LSI)) * WakeUpCounter
==> WakeUpCounter = Wakeup Time / Wakeup Time Base
To configure the wake up timer to 4s the WakeUpCounter is set to 0x1FFF:
RTC_WAKEUPCLOCK_RTCCLK_DIV = RTCCLK_Div16 = 16
Wakeup Time Base = 16 /(~39.000KHz) = ~0,410 ms
Wakeup Time = ~4s = 0,410ms * WakeUpCounter
==> WakeUpCounter = ~4s/0,410ms = 9750 = 0x2616 */
HAL_RTCEx_SetWakeUpTimer_IT(&RTCHandle, 0x2616, RTC_WAKEUPCLOCK_RTCCLK_DIV16);
/* Insert 5 seconds delay */
HAL_Delay(5000);
/* Clear all related wakeup flags */
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU);
HAL_RTC_DeInit(&hrtc);
while (1)
{
HAL_Delay(10000);
/* Request to enter STANDBY mode (Wake Up flag is cleared in PWR_EnterSTANDBYMode function) */
HAL_RTC_Init(&hrtc);
HAL_PWR_EnterSTANDBYMode();
}
}
2019-01-24 2:56 AM
Hello,
Why you do not set the wake up time by setting the wake counter in the HAL_RTCEx_SetWakeUpTimer_IT function.
Instead of adding the "HAL_Delay" function, you can simply customize your wake up time like this:
- For example if you want to waking-up the MCU after 10 seconds:
You need just to calculate the value that you want to set.
Best Regards,
Mohamed Aymen.
2024-02-20 8:31 PM
If I want MCU to go to standby/stop mode for 10 hours, the counter value should be
However, it does not work. In my test, MCU wakes up just a few seconds nor matter how big WakeUpCounter is assigned.
2024-04-10 5:56 AM
Hello @HDaji.1
For the WakeUpCounter you have to take into account the counter deepth and the clock.
If you use RTC_WAKEUPCLOCK_RTCCLK_DIV2 as the clock, then you'll just have 2^16 * (2/32000) ≈ 4s, 32000 here is my origine clock (32K LSI), si it can change according to your situation.
But if you use RTC_WAKEUPCLOCK_CK_SPRE_16BITS (1Hz clock), then you can last 2^16 / (1Hz * 3600s) ≈ 18.2 hours.
And if you want to go even further, you can use RTC_WAKEUPCLOCK_CK_SPRE_17BITS (0.5Hz), and you will be able to last 2^16 / (0.5Hz * 3600s) ≈ 36.4 Hours.
So, if you want to stop for 10 hours, you can use :
HAL_RTCEx_SetWakeUpTimer_IT(&hrtc, 36000, RTC_WAKEUPCLOCK_CK_SPRE_16BITS, 36000);
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.