2020-12-14 1:40 PM
Hi. I try to use an external IDE, code::blocks in this case, but have some issues attaching to target. First, i took the gnutools and ST Link GDB server from CubeIDE 1.5.0 etc. (Since i know some needs to ask why I wont't use CubeIDE, the answser i simple, I simply do not like eclipse and eclipse does not like me)
When initializing a debug session from CubeIDE, it runs the Cubeprogrammer after the debugger is attached and which loads the memory
But it referees to a .srec file I do not find (ST-LINK_GDB_server_bwMwVC.srec)
What and where is this file?
I also try to find the command parameters sent to the cubeprogrammer, but Have no luck so far.
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_bwMwVC.srec
File : ST-LINK_GDB_server_bwMwVC.srec
Size : 264405 Bytes
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 2]
Download in Progress:
File download complete
Time elapsed during download operation: 00:00:04.866
Verifying ..For now I am only able to start the ST LINK gdb server and to start the gdb, I may run the code and pause it, but no breakpoints are loaded and I may not see the code since the above part is still missing in my code::blocks setup.
I need to figure out the parameters sent to the cube-programmer to load memory etc. the same way cubeide does it.
EDIT:
I managed to copy the .srec intermediate file from temp folder while it existed. But I do not understand why CubeIDE must create a Motorola S record file to load the device? Shouldn't the cubeprogrammer be able to use other formats like hex, bin and elf?
I have also played with the cube programmer parametres, but I have dificulties attaching to stlink using the -c option. For usb, which port to use. I have tried several but the target is not found. Below example is the last one i tested to se if port usb could be used as an input for the programmer to find any device connected to usb, which is a methode used by other debuggers, but to no help.
STM32_Programmer_CLI -c port=usb
2020-12-15 4:00 PM
For those interested
Found which options that CubeIDE used as input to STM32_Programmer_CLI
Now I am able to debug using code::block. I may not use SVD files at the moment but there exists a plugin somewhere that will enable this feature.
The following is the commands executed before gdb connects to the server and target.
killall ST-LINK_gdbserv
./STM32_Programmer_CLI --connect port=SWD mode=UR reset=hwRst --download Z045.srec --verify --quietmode
./ST-LINK_gdbserver -c ./config.txt &
sleep 1I have gained one new issue though after getting rid of eclipse, this is an unexpected crash at a certain point in my code. The strange thing is that the code compiles exatly the same both in CubeIDE and when using the self-sustained makefile (build flags and linking are the same). When debugging using CubeIDE, the very same code does not crash the MCU
;179: c = *pC;
0x8032ad6 ldr r3, [r7, #32] <----- Crashes
0x8032ad8 ldrb r3, [r3, #0]
0x8032ada strb r3, [r7, #22]To figure out what may cause this is my next project.
2020-12-15 5:18 PM
I find it much easier to use Visual Studio.
using the GPDSC toolchain option in the project manager
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.