2018-03-27 3:57 AM
I created support request, got proposed solution to it and I'd like to add a clarification to my question. However, I have no idea how to do it.
I can:
- accept solution (to soon)
- reject solution (not exactly what I want)
- update
I choose update, it seems to mean 'update your original request'. I added some text, pressed 'Send' and nothing changed. I tried to do it twice.
I feel very stupid but now I need technical support on how to use technical support -_-' What should I do if I need to post an answer to my support request without chaning its status or rewriting original question?
#st-support #technical-supportSolved! Go to Solution.
2018-03-27 9:47 AM
ahh.. your ticket is in 'Solution Proposed' status, i.e. ST Support already has answered your request. In this case I suggest to REJECT and then enter your comment before you SEND
2018-03-27 4:26 AM
I feel very stupid but now I need technical support on how to use technical support
Don't - the user interaction on that form is pretty poor.
I think you probably do need to reject the solution - even though that does seem a bit OTT.
2018-03-27 7:05 AM
yes, user interface is poor :( , but UPDATE function usually works. You just enter text or attach file and then click SEND. Please provide ticket number (TECHxxxx), then I will gladly verify if ticket has been updated in our system.
2018-03-27 9:12 AM
TECH049479
2018-03-27 9:47 AM
ahh.. your ticket is in 'Solution Proposed' status, i.e. ST Support already has answered your request. In this case I suggest to REJECT and then enter your comment before you SEND
2018-03-27 10:18 AM
Thank you, looks like it worked!
Interface is just insane (and really slow btw), especially compared to this forum.
2018-03-27 10:42 AM
yes agreed. Our OLS is based on ancient platform and will be replaced very soon (almost ready for launch).
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.