STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Does STM32F103RC support UBS host?

Posted on March 28, 2018 at 06:26Hi, I want to do a confirm that does STM32F103RC support USB host? I want to use STM32F103RC to connect to camera,  STM32F103RC can control camera to take picture and get this picture.

Change I2C speed on STM32

Posted on March 27, 2018 at 19:29Hi there,Is it possible to change the i2c bus speed dynamically after it has been initialized?Kind regards,#i2c #stm32

Ted NIVAN by Associate II
  • 1405 Views
  • 1 replies
  • 0 kudos

STM32F030F4P6 StandByMode power consumption

Posted on March 28, 2018 at 01:05Any ideas why this board consumes 3.3 mA in StandByMode even if there's nothing plugged in? I already desoldered the AMS1117 and the on board leds.Same goes for the STM32F103C8T6 I have. Both using around 3-4mA even ...

0690X00000604VqQAI.jpg
rtek by Associate II
  • 1015 Views
  • 0 replies
  • 0 kudos

What is ''Reset temporization''

Posted on March 27, 2018 at 12:44Hello,STM32 parts define a Reset temporization time (T RSTTEMPO) several 100 us long up to 4.5 ms on STM32F103. I did not find an explanation for this time, but I suspect this is the time from the nRST Pin reaching a...

How to read the IDR of portc for STM32F103R4

Posted on March 26, 2018 at 20:32 Hi I'm using STM32F103R4 and trying to read the IDR of portc but it only i get data for PC4 & PC5, so how i can figure it out below my configuration GPIO_InitTypeDef GPIO_InitStructure; RCC_APB2PeriphClockC...

UART baudrate on STM32

Posted on March 27, 2018 at 19:33Hi there,Is it possible to change the uart baudrate dynamically after it has been initialized?Kind regards,#uart #stm32

Ted NIVAN by Associate II
  • 1987 Views
  • 3 replies
  • 0 kudos

Sending infos from computer via SPI or USB

Posted on March 23, 2018 at 08:59Hello everyone,I am currently working on a STM32F103RBT6 MCU on the OLIMEXINO-STM32 board : https://www.olimex.com/Products/Duino/STM32/OLIMEXINO-STM32/open-source-hardware .So far, I am sending and receiving CAN mes...

B C by Associate II
  • 5005 Views
  • 5 replies
  • 0 kudos

Resolved! How to use ST support form?

Posted on March 27, 2018 at 12:57I created support request, got proposed solution to it and I'd like to add a clarification to my question. However, I have no idea how to do it.I can:- accept solution (to soon)- reject solution (not exactly what I w...

amomum by Associate III
  • 3735 Views
  • 6 replies
  • 0 kudos

SPI RXONLY bit toggle when SPI is enabled

Posted on March 27, 2018 at 15:51Hello,Is it OK to toggle RXONLY bit when SPI is enabled? The reference manual on STM32 family says nothing special about this bit (in contrast to DFF and CRCEN), but when I configure SPI with RXONLY enabled and later...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.