2022-03-27 2:04 PM
UM2033 mentions that Wi-fi connector of stm32f769i-discovery development board can be configured for i2c board using signals EXT_SCL and EXT_SDA that are connected to PG3 and PG6, however datasheet of MCU (DS11532) these pins do not support I2C.
Is this configuration intended for a software solution?
2022-03-27 4:46 PM
It looks like you'd do this as bit-bang I2C,along with changing the solder bridges.
Not sure there are any examples where this is used.
If you need I2C perhaps use the D14/D15 on the Arduino connection PB9/PB8
2024-09-14 3:36 AM
Hello Tesla:
Since PB8 and PB9 have been used for other purposes, I can only use PG3 and PG6,the extension I2C connector.After I change the port to PG3 and PG6,how can I configure the port, but the interface will become low, so that it is always busy and cannot be used? I really need your help.Thanks.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.