2018-09-11 1:52 AM
Hello, I'm using the STM32746G Discovery Board to familiarize myself with the ST environment. Now I simply wanted to store a 32Bit value in the RAM, and had several problems with the Cube BSP drivers. I tested the functions with the following code:
#define SDRAM_OFFSET ((uint32_t)0xC0100000)
for(uint32_t i=0; i<0x10010; i++){
BSP_SDRAM_WriteData(SDRAM_OFFSET+i*4,(uint32_t *)&i,1);
}
for(uint32_t i=0; i<0x10010; i++){
testarray[i]= 0;
}
for(uint32_t i=0; i<0x10010; i++){
if(SDRAM_OK != BSP_SDRAM_ReadData(SDRAM_OFFSET+i*4,(uint32_t *)(&testarray[i]),1)){
testarray[i] = 111111;
}
}In the debugger it then looks like this:
Sometimes the transfer works. Sometimes the higher bits are incorrect.
How do I use the function to make it work?
Further I could not find out which SD-RAM area is used by the LCD driver. Which area can I overwrite without worrying about disturbing the display functions? Unfortunately I could not read this out of the code.
Solved! Go to Solution.
2019-01-16 4:52 AM
Okay, I think I'm getting closer to the problem. Obviously the problem is with the clock configuration. I'll look into it more closely and let you know better. Thank you very much for your help Clive Two.Zero.
I guess without it I would not have been able to get any further.
2019-01-16 5:00 AM
Clocks and other pin usage would be prime suspects.
2019-01-16 7:21 AM
As in many examples I found online the clocks are configured with a function void SystemClock_Config(void). To make the display work, I copied the function from an example. It caused the error in the SD-Ram write process. As I read from the comments, the SD-RAM can be operated up to a system clock of 200MHz. If I understood it correctly, mine has been set to 216MHz. Now I have the following clock configuration function:
void SystemClock_Config(void)
{
/**Macro to configure the PLL multiplication factor*/
__HAL_RCC_PLL_PLLM_CONFIG(16);
/**Macro to configure the PLL clock source*/
__HAL_RCC_PLL_PLLSOURCE_CONFIG(RCC_PLLSOURCE_HSI);
/**Configure the main internal regulator output voltage*/
__HAL_RCC_PWR_CLK_ENABLE();
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE3);
RCC_ClkInitTypeDef RCC_ClkInitStruct;
RCC_OscInitTypeDef RCC_OscInitStruct;
//RCC_PeriphCLKInitTypeDef PeriphClkInitStruct;
HAL_StatusTypeDef ret = HAL_OK;
/* Enable HSE Oscillator and activate PLL with HSE as source */
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
RCC_OscInitStruct.HSEState = RCC_HSE_ON;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
RCC_OscInitStruct.PLL.PLLM = 25;
RCC_OscInitStruct.PLL.PLLN =380;// old value: 400
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
RCC_OscInitStruct.PLL.PLLQ = 8;
ret = HAL_RCC_OscConfig(&RCC_OscInitStruct);
if(ret != HAL_OK){
_Error_Handler(__FILE__, __LINE__);
}
/* Activate the OverDrive to reach the 200 MHz Frequency */
ret = HAL_PWREx_EnableOverDrive();
if(ret != HAL_OK){
_Error_Handler(__FILE__, __LINE__);
}
/* Select PLL as system clock source and configure the HCLK, PCLK1 and PCLK2 clocks dividers */
RCC_ClkInitStruct.ClockType = (RCC_CLOCKTYPE_SYSCLK | RCC_CLOCKTYPE_HCLK | RCC_CLOCKTYPE_PCLK1 | RCC_CLOCKTYPE_PCLK2);
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;
ret = HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_6);
if(ret != HAL_OK){
_Error_Handler(__FILE__, __LINE__);
}
/**Configure the Systick interrupt time*/
HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000);
/**Configure the Systick*/
HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK);
/* SysTick_IRQn interrupt configuration */
HAL_NVIC_SetPriority(SysTick_IRQn, 0, 0);
}To make the diplay and RAM work, I changed the RCC_OscInitStruct.PLL.PLLN from 400 to 380. I guess more or less: PLLN = 400: 216MHz, so PLLN=380: 200MHz.
Find it difficult to read from the TRM which PLL is now responsible for what. If someone has a better solution, I would be interested in it. This has now solved the problem for me temporarily.
2019-01-16 9:05 AM
Yeah, I don't understand your frequency math there, or the use of the macros.
2019-01-17 1:52 AM
I thought if PLLN=400 is a multiplier that generates the 216MHz, then 380 => 216/400*380 = 205 MHz should be generated. A bit closer at 200MHz might be more precise expressed. At least it's working now. Even if I don't understand exactly what I changed in the clocks and what is affected by it.
2019-01-17 6:04 AM
Freq = ((HSE / M) * N) / P
25 MHz HSE is divided to 1 MHz for the comparison frequency
P is 2, turns VCO pulses to 50/50 duty clock
So
N=432 -> 216 MHz
N=400- > 200 MHz
N=380 -> 190 MHz
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.