cancel
Showing results for 
Search instead for 
Did you mean: 

How to setup timer to trigger ADC using STM32F051

Ngai yuk kong
Associate II
Posted on May 02, 2018 at 12:34

I know this is an old problem but I really cannot figure out.

My intention is to use timer 15 as a trigger source with setting equal to 1kHz. Then by enabling ADC interrupt using EOC  flag I think I could have an ADC interrupt of 1kHz used to convert 5 channels (they are not sampling at the same rate, so I want to use this ADC interrupt to set another time period.....)

I have the below source code: I could not enter the interrupt routine even one time. 

void initADC(void)

{

ADC1->CFGR1 =

_VAL2FLD(ADC_CFGR1_DISCEN, 1) | // discontinuous mode

_VAL2FLD(ADC_CFGR1_AUTOFF, 0) |

_VAL2FLD(ADC_CFGR1_WAIT, 0) |

_VAL2FLD(ADC_CFGR1_CONT, 0) |

_VAL2FLD(ADC_CFGR1_OVRMOD, 0) |

_VAL2FLD(ADC_CFGR1_EXTEN, 1) |

_VAL2FLD(ADC_CFGR1_EXTSEL, 4) |

_VAL2FLD(ADC_CFGR1_ALIGN, 0) | // data right aligned

_VAL2FLD(ADC_CFGR1_RES, 0) | // 12 bit resolution

_VAL2FLD(ADC_CFGR1_SCANDIR, 0) | // upward scan

_VAL2FLD(ADC_CFGR1_DMACFG, 1) | // DMA circular mode

_VAL2FLD(ADC_CFGR1_DMAEN, 0); // DMA disabled

ADC1->CFGR2 |= ADC_CFGR2_CKMODE_0;

// sampling time set to 28.5 ADC clock cycles:

ADC1->SMPR = _VAL2FLD(ADC_SMPR_SMP, 3);

//I have 5 channels but just test one channel first

ADC1->CHSELR = ADC_CHSELR_CHSEL1; //| //PA1

//ADC_CHSELR_CHSEL8 | //PB0

//ADC_CHSELR_CHSEL9; //PB1

ADC1->IER |= ADC_IER_EOCIE;

cfp_SetBit(&ADC1->ISR, ADC_ISR_ADRDY); // clear ready flag

cfp_SetBit(&ADC1->CR, ADC_CR_ADEN);

while (!cfp_IsBitSet(ADC1->ISR, ADC_ISR_ADRDY)) {

;

}

cpu_EnableInterrupt(ADC1_COMP_IRQn);

//init timer 15

TIM15->PSC = 47;   //48MHz / 48

TIM15->ARR = 999; //set to 1kHz

TIM15->CCR2 |= TIM_CR2_MMS_1;

TIM15->EGR |= TIM_EGR_UG;

TIM15->CR1 |= TIM_CR1_CEN;

cfp_SetBit(&ADC1->ISR, ADC_ISR_EOS); // clear end of sequence flag

cfp_SetBit(&ADC1->CR, ADC_CR_ADSTART);

}

void ADC1_COMP_IRQHandler(void)

{

   if( (ADC1->ISR & ADC_ISR_EOC) )

   {

   ADC1->ISR &= ~(ADC_ISR_EOC);

   digio_ToggleOutputValue(GPIOB, 14);

   }

}

Thank you in advance for any help...........

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Ngai yuk kong
Associate II
Posted on May 03, 2018 at 05:19

I solve it, thanks all.

Posted on May 07, 2018 at 12:14

Hello

paul.ngai

,

It will be more interesting to let us know how you resolved this issue. It may be helpful for forum users.

Best Regards,

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Apill
Senior

@Imen DAHMEN, There is also a video in youtube with the key word ADC TIMER

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.