STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to setup timer to trigger ADC using STM32F051

Posted on May 02, 2018 at 12:34I know this is an old problem but I really cannot figure out.My intention is to use timer 15 as a trigger source with setting equal to 1kHz. Then by enabling ADC interrupt using EOC  flag I think I could have an ADC in...

LSE Clock Output Missing Pulses on NUCLEO-F767ZI

I used STM32CubeMX to build a very simple test case to output both the High Speed Clock (HSE) and Low Speed Clock (LSE) on output pins. I selected "Master Clock Output 1" and Master Clock Output 2" when I configured the input clocks. The HSE clock ...

MPatt.11 by Associate II
  • 5807 Views
  • 6 replies
  • 0 kudos

[STM32L082] Powering the USB section of the chip

I do not want to use the USB part of the STM32L082. According to the Ref Manual RM0376 page 140 there is no explicit mention that the VCC_USB can be tied to GND if not in use. So what would be the thing to do (and reduce the power even further): GND ...

No MOSI PULSE if use SPI re-mapped

Posted on February 28, 2013 at 04:03A am using STM32F103T4, a low density device, and want to use the re-mapped SPI1. Below is my implementation:  /* GPIO and AFIO clock enable */  RCC_APB2PeriphClockCmd(RCC_APB2Periph_AFIO| RCC_APB2Periph_GPIOB, EN...

ronrafer by Associate
  • 982 Views
  • 2 replies
  • 0 kudos

STM32L051 TIM21 trigger output issue

Hi,Using the following code, ADC can be triggered by TIM22 successfully./** * @fn static void ADC_Config(void) * * @brief ADC configuration. */ static void ADC_Config(void) { /* Enable clock */ RCC->AHBENR |= RCC_AHBENR_DMAEN; RCC-...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.