2019-05-01 6:02 PM
Hi guys, I have a project where I need to use STM32 ARM processors I want to be able to program a bare chip of STM32's ARM Microcontrollers on my breadboard. I have a ST link V2 as the programmer. I would like to know what software (for free only)/application I need to install on my computer to code and upload it to this bare chip of mine. What are the steps I need to take to successfully write code and dump it on my STM32 ARM Microcontroller.
To basically sum it up, I have a LCD display, and I want to display characters from a sensor's readings, so which software do I use to write and upload code and it should be used with my ST link v2.
Thank you.
2019-05-01 9:31 PM
If you want to work with HAL library then use STM32CUBEMX which is free of cost, this help you to make skeleton of program . You can also use Standard Peripheral library which is easy but take time to understand. IDE you can use KEIL, ATOLIC, SYTEMWORK BENCH and CoCox. its depend on you.
2019-05-01 9:35 PM
Which type of LCD is that means 16x2 or graphical type.
2019-05-01 10:08 PM
its a 16x2 LCD display
2019-05-01 10:10 PM
Where can I download Keil from? what is the exact software I need to use?
2019-05-02 9:51 PM
Does a bare STM32 ARM chip come with a boot loader installed? or do I need to program one for it to work? Whats the procedure to do it?
2019-05-02 10:05 PM
Below is arm keil link download from here:-
https://www2.keil.com/stmicroelectronics-stm32/mdk
For interfacing of 16x2 LCD you got support from youtube or by github.
2019-05-02 10:27 PM
Can I follow the same code as what this video shows? (look at 5:27 for what I am talking about) https://www.youtube.com/watch?v=877SPdwuuLA&list=PL6PplMTH29SHgRPDufZhfMRoFwRAIrzOp&index=27
And does a bare chip from STM come with the boot loader installed or do I have to make my own boot loader program?
2019-05-07 11:02 AM
Sorry for late reply.
This tutorial is good.
Actually I will suggest that if you will see his all tutorial of arm series that is benefits for you because his tutorials are awesome.
2019-05-07 1:38 PM
Most (possibly all) STM32 microcontrollers come with a boot loader in flash ROM. The boot loader allows firmware programming via the microcontroller's USART(s), often also USB, and other peripherals.
ST provides a Windows application called STM32CubeProgrammer that can program firmware into the microcontrollers.
Of course, the ST Link can also do this.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.