2017-10-25 2:43 AM
Hello everybody:
I would like to multiply the outputs I get from TIM3_PWM (64KHz signal) and TIM4_PWM(8MHz signal) in order to get a new signal.
The thing is that I don�t know how to do it and I�m pretty lost.
By the way is it possible to assign variables to the timers? and if so, how can I do it?
Thank you in advance.
Endika
#timer #stm32-f4 #tim #multiply #variable2017-10-25 3:22 AM
You can set TIM4's OCxREF as TRGO in TIM4_CR2.MMS, set TIM3's TRGI source to TIM4 in TIM3_SMCR.TS, and set TIM3 slave controller to Gated Mode in TIM3_SMCR.SMS - that should suffice.
By the way is it possible to assign variables to the timers?
I don't understand, please explain.
JW
2017-10-26 5:03 AM
Yes, I´m asking if this is possible:
HAL_TIM_PWM_Start(&htim3,TIM_CHANNEL_2) = a;
For example
2017-10-26 5:13 AM
No.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.