2025-03-25 7:45 AM
Hi,
I am using the STM32U575.
In my application, I have to transfer ADC readings to a destination buffer. I have set the DMA source address to the ADC data register (16-bit), and the destination address to a memory buffer start address. The data width is 16-bits or half word, as per the STM32 size definitions.
My requirement is that I need to fill the ADC 1024 samples into the memory and after receiving these, transfer them to another buffer, that is connected to a UART, to be transmitted out.
However, I need to increment the DMA destination buffer address by 32 bits, after each sample from the ADC, meaning, leave alternate half words empty.
The data would look like this in the memory buffer:
ADDR 0: fill with sample 1 (16 bits) - increment DMA destination address by one word (32-bits)
ADDR 2: empty - 16- bits
ADDR4: fill with sample 2 (16 bits) - increment DMA destination address by one word (32-bits)
ADDR6: empty - 16 bits
........
and so on till the 1024th location.
But in the DMA settings, the address increment value options do not have such a choice.
Is there any way to achieve this?
Any ideas are welcome .. :)
Solved! Go to Solution.
2025-03-25 12:35 PM
If you're using DMA in circular mode, then no. You'll have to copy the HT/TC data to another buffer.
If using Normal mode, then after each callback, you can pass the memory address to the DMA for the next conversion.
Why don't you just put the ADC data into a UART transmit buffer on each callback? Then in your polling routine you can transmit the available data in the transmit buffer. The receiving end can have queues of 1024 packets. So as 1 queue is being parsed, the other queue(s) are being filled.
2025-03-25 12:35 PM
If you're using DMA in circular mode, then no. You'll have to copy the HT/TC data to another buffer.
If using Normal mode, then after each callback, you can pass the memory address to the DMA for the next conversion.
Why don't you just put the ADC data into a UART transmit buffer on each callback? Then in your polling routine you can transmit the available data in the transmit buffer. The receiving end can have queues of 1024 packets. So as 1 queue is being parsed, the other queue(s) are being filled.
2025-03-31 10:29 PM
Hello Karl,
I am using the suggesting you gave - about incrementing the DMA destination address in the ADC conversion complete callback and it works fine. Thank you !
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.