cancel
Showing results for 
Search instead for 
Did you mean: 

MULTI_Q U545REQ

dlagyals
Associate II

I used MultiQ example 'LPBAM_DMA_MultiQExec' 

I change code for U545REQ board but it doesn't work.

i found some issue

This is 'LPBAM_DMA_MultiQExec' code

tatic void MX_LPDMA1_Init(void)
{

  /* USER CODE BEGIN LPDMA1_Init 0 */

  /* USER CODE END LPDMA1_Init 0 */

  /* Peripheral clock enable */
  __HAL_RCC_LPDMA1_CLK_ENABLE();

  /* LPDMA1 interrupt Init */
    HAL_NVIC_SetPriority(LPDMA1_Channel0_IRQn, 0, 0);
    HAL_NVIC_EnableIRQ(LPDMA1_Channel0_IRQn);

  /* USER CODE BEGIN LPDMA1_Init 1 */

  /* USER CODE END LPDMA1_Init 1 */
  handle_LPDMA1_Channel0.Instance = LPDMA1_Channel0;
  handle_LPDMA1_Channel0.InitLinkedList.Priority = DMA_LOW_PRIORITY_LOW_WEIGHT;
  handle_LPDMA1_Channel0.InitLinkedList.LinkStepMode = DMA_LSM_FULL_EXECUTION;
  handle_LPDMA1_Channel0.InitLinkedList.LinkAllocatedPort = DMA_LINK_ALLOCATED_PORT1;
  handle_LPDMA1_Channel0.InitLinkedList.TransferEventMode = DMA_TCEM_LAST_LL_ITEM_TRANSFER;
  handle_LPDMA1_Channel0.InitLinkedList.LinkedListMode = DMA_LINKEDLIST_NORMAL;
  if (HAL_DMAEx_List_Init(&handle_LPDMA1_Channel0) != HAL_OK)
  {
    Error_Handler();
  }
  if (HAL_DMA_ConfigChannelAttributes(&handle_LPDMA1_Channel0, DMA_CHANNEL_PRIV) != HAL_OK)
  {
    Error_Handler();
  }
  /* USER CODE BEGIN LPDMA1_Init 2 */

  /* USER CODE END LPDMA1_Init 2 */

}

my generation code is

static void MX_LPDMA1_Init(void)
{
  /* USER CODE BEGIN LPDMA1_Init 0 */

  /* USER CODE END LPDMA1_Init 0 */

  /* Peripheral clock enable */
  __HAL_RCC_LPDMA1_CLK_ENABLE();

  /* USER CODE BEGIN LPDMA1_Init 1 */

  /* USER CODE END LPDMA1_Init 1 */

  /* Set LPDMA1 instance */
  handle_LPDMA1_Channel3.Instance = LPDMA1_Channel3;
  handle_LPDMA1_Channel3.InitLinkedList.Priority = DMA_LOW_PRIORITY_LOW_WEIGHT;
  handle_LPDMA1_Channel3.InitLinkedList.LinkStepMode = DMA_LSM_FULL_EXECUTION;
  handle_LPDMA1_Channel3.InitLinkedList.TransferEventMode = DMA_TCEM_LAST_LL_ITEM_TRANSFER;
  handle_LPDMA1_Channel3.InitLinkedList.LinkedListMode = DMA_LINKEDLIST_CIRCULAR;
  if (HAL_DMAEx_List_Init(&handle_LPDMA1_Channel3) != HAL_OK)
  {
    Error_Handler();
  }
}

 why ' handle_LPDMA1_Channel3.InitLinkedList.LinkAllocatedPort = DMA_LINK_ALLOCATED_PORT1;' This line is not generatione??

2 REPLIES 2
dlagyals
Associate II

This is my file. please help me

dlagyals
Associate II

Is there no one? No one is responding??

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.