2025-07-10 2:57 AM
First of all, I am not using CUBE IDE, this is a bare metal.
Second: STM32H523. ADC (continuous mode; DMA). ADC is configured on PA0 (i.e. INP1, single-ended), GPIO configuration is analog mode.
On the pin I can probe (oscilloscope) my signal (correct amplitude): a sinus. But the data (from DMA) is noise.
Configured with PA1, all works fine (so my soft is ok). Using ADC1 or ADC2 does not change anything.
Second observation: with PA0, the DC is not fixed (floating pin), but configured on PA1, the pin is DC-driven (about VDDA/2, high impedance).
=> For these reasons, I have the feeling PA0 is not connected to ADC. I can't find anything in registers/documentation/erratas explaining this (on H7 there is some analog switches, but nothing for H5).
Any clue? Thanks!
Solved! Go to Solution.
2025-07-10 3:21 AM
Hello @jeremierafin
Please verify that the OP0 bit in the ADC_OR register is actually set to 1 after initialization.
Kind regards,
2025-07-10 3:21 AM
Hello @jeremierafin
Please verify that the OP0 bit in the ADC_OR register is actually set to 1 after initialization.
Kind regards,
2025-07-10 3:37 AM
Actually, that was my missing configuration :)
Thanks a lot!!!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.