2019-05-10 3:23 AM
Hi,
I am working on STM32F56G eval board. I need to generate a PWM pulse with varying time period on a single channel. I am new to stm32 PWM. With DMA burst code example time period is changing on the runtime .
How can I generate a PWM pulse with different time period on a single channel?
Eg : 1 pulse (x time period) + 2 pulse (y time period) +3 pulse (x time period)
If it is possible to generate such PWM pulse pattern then please suggest approach or example code.
Any help is appreciated.
2019-05-10 10:51 AM
Chose a timer with DMA channel on the channel, and define a marco period of 6 pulse period.
Use the DMA cyclic table to go through the 12 toggle events.
Is this what you need implemented?
2019-05-12 9:46 PM
Thanks.
I want to implement a pattern of pulse with varying time periods.
A output on oscilloscope should be like :
A pulse (1Khz) + delay (200ms) + pulse (2KHz) +..
Where I need to add delays between pulses.
Any steps to achieve such a pattern is helpful.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.