2020-01-29 2:42 PM
I am using the STM32G071RB board; trying to enter standby mode and wakeup using the automated timer after a certain number of seconds. I can't find any documentation on what I need to enable/disable before entering standby mode and attempting to wakeup on interrupt. I am using the following sequence but am not seeing the board actually go into standby mode and then wakeup. Any suggestions would be appreciated.
int main(void)
{
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* Configure the system clock */
SystemClock_Config();
/* Initialize all configured peripherals */
MX_RTC_Init();
// Enable Power Control clock //
__HAL_RCC_PWR_CLK_ENABLE();
/* Check and handle if the system was resumed from StandBy mode */
if (__HAL_PWR_GET_FLAG(PWR_FLAG_SB) != RESET) {
/* Clear Standby flag */
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_SB);
// Check and Clear the Wakeup flag
if (__HAL_PWR_GET_FLAG(PWR_FLAG_WUF) != RESET) {
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_WUF);
}
}
/* Disable Wakeup Counter */
HAL_RTCEx_DeactivateWakeUpTimer(&hrtc);
HAL_RTCEx_PollForWakeUpTimerEvent(&hrtc,Timeout);
HAL_RTCEx_SetWakeUpTimer_IT(&hrtc, 0x2616, RTC_WAKEUPCLOCK_RTCCLK_DIV16);
/* Clear all related wakeup flags */
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_WUF);
HAL_RTC_Init(&hrtc);
HAL_PWR_EnterSTANDBYMode();
/* Infinite loop */
while (1) {
}
}
// This Callback function is below and outside int main()
void HAL_RTCEx_WakeUpTimerEventCallback(RTC_HandleTypeDef *hrtc)
{
/* Prevent unused argument(s) compilation warning */
UNUSED(hrtc);
/* NOTE : This function should not be modified, when the callback is needed,
the HAL_RTCEx_WakeUpTimerEventCallback could be implemented in the user file
*/
HAL_Delay(5000);
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.