2008-11-13 5:29 PM
How to convert a (u32 *) to (u8 *)???
2011-05-17 3:52 AM
Hi Relaxe,
u8 *buffer8;u32 *buffer32;
buffer8 = (u8*)buffer32;sword_82
2011-05-17 3:52 AM
Ok, this question is rather simple.
the SDIO+SDCard example's functions give their result in a 32bit pointer, like: u32 *readbuff. Now, I want to implement a filesystem library like dosfs or efsl. They all require to have a read/write function wich use a 8 bit pointer, like: u8 *buffer. Now, is there an easy way to pass/convert one to another, without have to transfer the u32* buffer to another u8*buffer 8bits at a time? I was looking at something like ''u8 *buffer8 = (u8 *) buffer32'' .... Is it doable? Thanks! -Relaxe2011-05-17 3:52 AM
Thanks Sword!
Now, this actually works: u32 Buffer32[2] = {0x33323130, 0x37363534}; u32 *PtrBuffer32 = Buffer32; u8 *PtrBuffer8; PtrBuffer8 = (u8*) PtrBuffer32; printf(''%d\n'', *(PtrBuffer8+0)); printf(''%d\n'', *(PtrBuffer8+1)); printf(''%d\n'', *(PtrBuffer8+2)); printf(''%d\n'', *(PtrBuffer8+3)); printf(''%d\n'', *(PtrBuffer8+4)); printf(''%d\n'', *(PtrBuffer8+5)); And as you can see, I'm not recreating a whole new buffer, just changing the pointer :p -Relaxe [ This message was edited by: relaxe on 13-11-2008 16:33 ]2011-05-17 3:52 AM
Quote:
I'm not recreating a whole new buffer, just changing the pointer
You probably don't even need to change the pointer - just the cast should do it. However, this is not so simple in the other direction; ie, from a u8* to a u32* pointer - because of the alingment requirements of multi-byte objects... [ This message was edited by: st7 on 14-11-2008 01:52 ]2011-05-17 3:52 AM
You may find this general purpose cast macro to be useful
/* Thanks to SM Ryan who provided the * LV macro in news:comp.lang.c * As given, the macro name was lvaluecast * Message-ID: */ #define LV(type,lvalue) (*((type*)((void*)(&(lvalue))))) I used it to store an int to a *int like this LV(int*,sp) -= extraStackSpace;We’re moving the ST Community to a new platform to give you a better and more reliable community experience.