2008-11-12 7:14 AM
GPIO Configuration
2011-05-17 3:52 AM
If you have two conflicting peripherals and you remap your GPIO to support one, but not the other, is it possible to still use the other peripherial?
In the case of a timer, if you don't map all of its channels to a GPIO pin, can you still use those channels internally? Has anyone did any experimenting with this or is there a document that addresses this issue? thanks2011-05-17 3:52 AM
Hi ,
Have a look at : http://www.st.com/mcu/forums-cat-6268-23.html http://www.st.com/mcu/forums-cat-6399-23.html ST1.2011-05-17 3:52 AM
Thanks for the links.
From what I gathered so far, if I'm using USART1 and I don't remap TIM1, I could have a conflict if both peripherals are active. There isn't a way to use TIM1's channel 1 and 2 internally without expecting TIM1 to affect the external pins. So in the case of the AF remap and debug I/O configuration register, if neither USART1 or TIM1 is remapped, I can expect to see an ORed result from TIM1 and USART1 on the shared output pins?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.