2019-11-23 11:31 AM
Hi,
i am using STM32F407 and CubeIDE. I am trying to use 1 master and 2 slave at the same time. I can connect any slave to the master. I am trying to implement a sinmple alghoritm for 2 slaves. I change device address which master is connected at 10 seconds interval.And when i try to connect both of them at the same time, my master always stays in AT Mode. It doesn't never blink fast (when it bilnks fast, it indicates that it is not in AT mode and searching for a device). Also my slave sends data. What is the problem with master?
Here is datasheet: https://components101.com/sites/default/files/component_datasheet/HC-05%20Datasheet.pdf
int main(void)
{
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_USART6_UART_Init();
HAL_GPIO_WritePin(GPIOC, GPIO_PIN_0, GPIO_PIN_SET); //Reset HC-05
HAL_Delay(1000);
HAL_GPIO_WritePin(GPIOC,GPIO_PIN_1,GPIO_PIN_SET);// set high to 'key' pin to enter AT Mode
HAL_Delay(1000);
HAL_GPIO_WritePin(GPIOC, GPIO_PIN_0, GPIO_PIN_RESET);//set low to reset pin
HAL_Delay(3000);
HAL_UART_Transmit(&huart6,(uint8_t*)"AT+ROLE=1\r\n",sizeof("AT+ROLE=1\r\n")-1,100);
HAL_Delay(1000);
HAL_UART_Transmit(&huart6(uint8_t*)"AT+CMODE=0\r\n",sizeof("AT+CMODE=0\r\n")-1,100);
HAL_Delay(1000);
HAL_GPIO_WritePin(GPIOC, GPIO_PIN_0, GPIO_PIN_SET);
HAL_GPIO_WritePin(GPIOC, GPIO_PIN_0, GPIO_PIN_RESET);//exit AT mode
/* USER CODE BEGIN 2 */
__HAL_UART_ENABLE_IT(&huart6,UART_IT_RXNE); //enable usart interrupt
/* USER CODE END 2 */
while (1)
{
/* FIRST SLAVE */
HAL_GPIO_WritePin(GPIOC, GPIO_PIN_0, GPIO_PIN_SET);
HAL_Delay(1000);
HAL_GPIO_WritePin(GPIOC,GPIO_PIN_1,GPIO_PIN_SET);
HAL_Delay(1000);
HAL_GPIO_WritePin(GPIOC, GPIO_PIN_0, GPIO_PIN_RESET);//i entered AT mode to change slave addres
HAL_UART_Transmit(&huart6(uint8_t*)"AT+BIND=98D3,31,F63543\r\n",sizeof("AT+BIND=98D3,31,F63543\r\n")-1,100); //address of slave
HAL_GPIO_WritePin(GPIOC, GPIO_PIN_0, GPIO_PIN_SET);
HAL_GPIO_WritePin(GPIOC, GPIO_PIN_0, GPIO_PIN_RESET);//exit AT mode
HAL_Delay(50000);//wait for data transmission
/*SECOND SLAVE */
HAL_GPIO_WritePin(GPIOC, GPIO_PIN_0, GPIO_PIN_SET);
HAL_Delay(1000);
HAL_GPIO_WritePin(GPIOC,GPIO_PIN_1,GPIO_PIN_SET);
HAL_Delay(1000);
HAL_GPIO_WritePin(GPIOC, GPIO_PIN_0, GPIO_PIN_RESET);//i entered AT mode to change slave addres
HAL_UART_Transmit(&huart6(uint8_t*)"AT+BIND=98D3:31:F537A2\r\n",sizeof("AT+BIND=98D3:31:F537A2\r\n")-1,100); //address of slave
HAL_GPIO_WritePin(GPIOC, GPIO_PIN_0, GPIO_PIN_SET);
HAL_GPIO_WritePin(GPIOC, GPIO_PIN_0, GPIO_PIN_RESET);//exit AT mode
HAL_Delay(50000);//wait for data transmission
}
}Slave configuration:
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_1, GPIO_PIN_SET);// reset hc-05
delay_ms(1000);
HAL_GPIO_WritePin(GPIOA,GPIO_PIN_7,GPIO_PIN_SET);// set high to 'key' pin to enter AT
delay_ms(1000);
HAL_GPIO_WritePin(GPIOB,GPIO_PIN_1,GPIO_PIN_RESET);// entered AT mode
delay_ms(3000);
HAL_UART_Transmit(&huart1,(uint8_t*)"AT+ROLE=0\r\n",sizeof("AT+ROLE=0\r\n")-1,100);
delay_ms(1000);
HAL_GPIO_WritePin(GPIOB,GPIO_PIN_1,GPIO_PIN_SET);
HAL_GPIO_WritePin(GPIOB,GPIO_PIN_1,GPIO_PIN_RESET);//exit AT mode
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.