2021-10-18 10:41 PM
If I vary any one channel Input through POT, it is reflecting in another ADC Channel also... can anyone help me regarding this ?
2021-10-19 9:38 PM
Sure Thanks for the Suggestion..
along with this i will try to use configurations with another channels too
Will update you , Incase If I need any help regarding this, Thanks again @Georgy Moshkin
2021-10-20 10:39 AM
Is There any function to disable Specific ADC Channel after Analog to Digital Conversion
@Georgy Moshkin
2021-10-20 6:54 PM
Most straight forward way is de-initializing/stopping peripheral using functions like HAL_ADC_DeInit(), and then initializing/starting again with new parameters. Some things may be performed without de-initialization, bust must dig into reference manual to find out, some hints may be found in HAL source code comments (stm32..._hal_adc.c).
2021-10-21 5:21 AM
Should I select another controller which is Having Two ADC's(ADC1,ADC2) and CAN Protocol, If you know any controller having this features suggest me ?
@Georgy Moshkin
2021-10-21 6:43 AM
Probably no, there are a lot of channels, select channels and make sure those pins are not used on your Nucleo board for something else, or remove solder bridges according to Nucleo documentation
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.