2021-07-27 7:24 AM
Hello Everyone,
I have Nucleo-H723ZG and I managed to configure CAN to work there but only sending messages. I am not able to get anything in RX Buffer.
I configured CAN like:
hfdcan1.Instance = FDCAN1;
hfdcan1.Init.FrameFormat = FDCAN_FRAME_CLASSIC;
hfdcan1.Init.Mode = FDCAN_MODE_EXTERNAL_LOOPBACK;
hfdcan1.Init.AutoRetransmission = ENABLE;
hfdcan1.Init.TransmitPause = DISABLE;
hfdcan1.Init.ProtocolException = DISABLE;
hfdcan1.Init.NominalPrescaler = 30;
hfdcan1.Init.NominalSyncJumpWidth = 2;
hfdcan1.Init.NominalTimeSeg1 = 19;
hfdcan1.Init.NominalTimeSeg2 = 12;
hfdcan1.Init.DataPrescaler = 1;
hfdcan1.Init.DataSyncJumpWidth = 1;
hfdcan1.Init.DataTimeSeg1 = 1;
hfdcan1.Init.DataTimeSeg2 = 1;
hfdcan1.Init.MessageRAMOffset = 0;
hfdcan1.Init.StdFiltersNbr = 128;
hfdcan1.Init.ExtFiltersNbr = 0;
hfdcan1.Init.RxFifo0ElmtsNbr = 0;
hfdcan1.Init.RxFifo0ElmtSize = FDCAN_DATA_BYTES_8;
hfdcan1.Init.RxFifo1ElmtsNbr = 0;
hfdcan1.Init.RxFifo1ElmtSize = FDCAN_DATA_BYTES_8;
hfdcan1.Init.RxBuffersNbr = 64;
hfdcan1.Init.RxBufferSize = FDCAN_DATA_BYTES_8;
hfdcan1.Init.TxEventsNbr = 32;
hfdcan1.Init.TxBuffersNbr = 32;
hfdcan1.Init.TxFifoQueueElmtsNbr = 32;
hfdcan1.Init.TxFifoQueueMode = FDCAN_TX_FIFO_OPERATION;
hfdcan1.Init.TxElmtSize = FDCAN_DATA_BYTES_8;
if (HAL_FDCAN_Init(&hfdcan1) != HAL_OK)
{
Error_Handler();
}Then I Initialize RX BUFFER:
sFilterConfig.IdType = FDCAN_STANDARD_ID;
sFilterConfig.FilterIndex = 0;
sFilterConfig.RxBufferIndex = 0;
sFilterConfig.FilterConfig = FDCAN_FILTER_TO_RXBUFFER;
sFilterConfig.FilterID1 = 0x100;
sFilterConfig.IsCalibrationMsg = 0;
if (HAL_FDCAN_ConfigFilter(&hfdcan1, &sFilterConfig) != HAL_OK)
{
Error_RXBuff(id);
}
if (HAL_FDCAN_ConfigGlobalFilter(&hfdcan1, FDCAN_REJECT, FDCAN_REJECT, FDCAN_FILTER_REMOTE, FDCAN_FILTER_REMOTE) != HAL_OK)
{
Error_Handler();
}
/* Start the FDCAN module */
if (HAL_FDCAN_Start(&hfdcan1) != HAL_OK)
{
Error_Handler();
}Problem is that I can not recieve anything in that RXBUFFER.
To recieve I use:
if(HAL_FDCAN_IsRxBufferMessageAvailable(&hfdcan1, 0))
{
FDCAN_RxHeaderTypeDef RxHeader;
HAL_FDCAN_GetRxMessage(&hfdcan1, 0, &RxHeader, data);
if(RxHeader.Identifier != 0)
{
*id = RxHeader.Identifier;
return HAL_OK;
}
return HAL_ERROR;
}What I do wrong with Recieve Buffer deffinition?
Sending messages works perfectly for me:
uint8_t CAN_putd(FDCAN_HandleTypeDef *hfdcan, uint32_t id, uint8_t *data, uint32_t buff)
{
FDCAN_TxHeaderTypeDef TxHeader;
TxHeader.Identifier = id;
TxHeader.IdType = FDCAN_STANDARD_ID;
TxHeader.TxFrameType = FDCAN_DATA_FRAME;
TxHeader.DataLength = FDCAN_DLC_BYTES_8;
TxHeader.ErrorStateIndicator = FDCAN_ESI_ACTIVE;
TxHeader.BitRateSwitch = FDCAN_BRS_OFF;
TxHeader.FDFormat = FDCAN_CLASSIC_CAN;
TxHeader.TxEventFifoControl = FDCAN_NO_TX_EVENTS;
TxHeader.MessageMarker = 0;
buff = 1<<buff; // TX Buffer represented in binary way
uint8_t status = HAL_OK;
status = HAL_FDCAN_AddMessageToTxBuffer(hfdcan, &TxHeader, data, buff);
if(status == HAL_OK)
{
status = HAL_FDCAN_EnableTxBufferRequest(hfdcan, buff);
}
return status;
}Regards,
Chris
Solved! Go to Solution.
2021-08-04 1:49 AM
2021-08-04 1:49 AM
Solved:
Simply use:
hfdcan1.Init.Mode = FDCAN_MODE_NORMAL;
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.