2021-07-27 12:51 AM
are the GPIOs at HI-z? pulled up? or Pulled down?
this is very important to me, I don't want to enable any circuit at start up.
2021-07-27 7:13 AM
Generally, they are in high impedance mode with no pullup/pulldown. Pins used for SWD/JTAG programming are the exception. The reference manual will provide this information in the GPIO registers section.
2021-07-28 9:51 PM
I tried to find it at the datasheet or application note, nothing about it.
where can I find explanation about it?
2021-07-29 12:37 AM
As TDK said:
The reference manual will provide this information in the GPIO registers section.
JW
2021-08-04 4:05 AM
Hi @IGAL TALOR ,
The application note STM32 GPIO configuration for hardware settings and low-power consumption (AN4899) should be useful for you.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.