2016-01-20 10:32 PM
I want to build my own board with in-built ST-LINK V2.
Just make it simpler. Assume we build a board exactly same as the discovery board. My question is how to program the chip STM32F103C8T6 to be a ST-LINK? As my understanding, STM32F103C8T6 is just a stm32 chip, we can program it using an external st-link via the pin PA13,PA14, those are JTMS, JTCK. Then the chip is ready as a st-link. Am I right? And where can i download the hex code for the chip STM32F103C8T6? Thanks2016-01-21 1:34 AM
The firmware of ST-Link is copyrighted proprietary product of ST. If you and your country's laws don't mind violating copyright, you can try to google these titles:
''Build a mini ST-LINK/V2 programmer/debugger for the STM32'' ''Retrieving ST-Link/V2 Firmware from Update Utility''2016-01-21 9:25 AM
Thanks for your reply. You are very helpful.
I don't mean to crack st-link. discovery board is everywhere and cheap. Any discovery board has a st-link on board, and st allows to use it as an external debugger.I am building my own development board. With in-built st-link, it would be more convenient to use. And it is simply for personal use only.On the other hand, if USA doens't allow to do this, I would stop on it.Thanks2016-01-21 10:29 AM
Remowe STM from STLink from some board or better solution is cat programmer part from nucleo.
I use this with changed connector.2016-01-21 12:00 PM
If you're just looking to integrate a debug probe / USB-serial adapter, there are some open source projects you could use that would give you similar functionality to an STLinkv2.
https://github.com/blacksphere/blackmagic/wiki/Hacking
http://akb77.com/g/stm32/cmsis-dap-adapter/
https://github.com/devanlai/dap42
(disclosure: this is my project)The two STLink features that you would be missing are:2016-01-21 1:21 PM
Thank you guys for your reply.
I just use it as a debugger.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.