2018-09-14 6:47 AM
Hi, I'm new in this world of ST. I have relative experience with Arduinos and LoRa, but now I want to do things with more resources. In particular, I am interested in the LoRa module from Murata and I bought the Discovery Kit B-L072Z-LRWAN1.
What I ask is a bit of guidance in this regard.
What IDE do you recommend? (I'm used to the Arduino IDE)
Where can I read things about it?
To program the B-L072Z-LRWAN1, I always prescribe the STLink or can I do it with a USB-Serial adapter?
A library to read a sensor (i2c for example) with the ide of Arduino can be used for this type of MCUs?
Any recommendation is welcome.
Thank you very much!
2018-09-14 8:39 AM
Suggest you use Keil, there are free licenses for ST Cortex-M0 parts, and significant clowning around compared to GNU/GCC - Eclipse platforms. Mileage varies, pick something you like.
The I-CUBE-LRWAN software has projects compilable with Keil
https://www.st.com/en/embedded-software/i-cube-lrwan.html
Review, build and test the projects provided, review context of code with respect to Semtech stack
The ST-LINK is the best way to program debug.
You can use the BOOT0 pin to get into the System Loader, and it's USART/USB programming modes.
Review AN2606 and related doc for the functions/protocols.
You'll have to code routines in HAL to talk to I2C peripherals.
Not familiar with ARM CPU, review Technical Reference Manuals, and supporting books like Joseph Yiu's Essential Cortex-Mx series. ST also has Data Sheets, Reference Manuals and Programming Manuals, review/skim those to understand the lay of the land and where to find detail if you need it.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.