2020-03-01 7:15 PM
I am considering powering a STM32G4 with a DC-DC Switching Converter. One of the converters I am looking at has a PWM Switching Frequency of 6-MHz, the other 500 kHz. I'd use a hefty inductor and capacitor to filter the current ripple at this PWM frequency out, but of course there will still be some ripple left in either case (note: the ripple at 6 MHz is significantly easier to filter out using a reasonably-sized inductor).
My main question is: How much current ripple at each of these frequencies is allowable when powering the VDD pins of a STM32?
Or, must I really use a dedicated LDO (for a cleaner VDD) for the STM32 instead? If not, is it at least advised to use an LDO for VDDA if doing ADC/DAC, but an adequately-filtered switching converter is ok for VDD? [Please just point me at the appropriate reference if this information is already published somewhere, I haven't yet found it.]
Thanks heaps - Tom
2020-03-02 1:34 AM
Strictly speaking you should be asking how much ripple voltage is tolerable at the Vdd and VddA pins.
Microcontrollers, indeed any digital CMOS, do not consume constant current. Instead take significant gulps of current for tiny durations (perhaps it is better to imagine they take gulps of charge), typically on every internal clock edge. The amount of each gulp depends on what processing is being done.
No voltage-regulator can respond fast-enough to these gulps. Indeed a few centimetres of pcb track has too much inductance to allow correct operation. So we put decoupling capacitors on every power-supply-pin pair on the stm32 package. The data sheet recommends 100 nF ceramic on each Vdd/Vss pair and one 4.7uF (could be tantalum or ceramic) - see the section on "power supply scheme".
These gulps are much bigger than likely ripple in a switch-mode regulator.
Ripple voltage might also affect the PLL oscillator stability but I haven't seen any data on that.
I have successfully used a TPS82150 switching-regulator module (built-in inductor) with 22 uF as the big decoupler and however many 100 nF.
As for VddA, ripple will have a direct bearing on ADC accuracy. So additional filtering is useful. Current drain might be sufficiently low that RC filtering is tolerable here. In my case I used 0.1 ohm and 10 uF.
Hope this helps,
Danish
2020-03-02 1:51 AM
The mcu's internal logic is powered through its own internal LDO.
JW
2020-03-04 12:34 PM
Recently, there was a thread on the STM32G4's ADC. The key takeaway for me was that Vref requires a low source impedance because during the conversion they need bursts of current. AN5346 talks about some of the requirements.
The Nucleo board schematic and the AN5346 schematic show an inductor with a short to bypass it - which tells me try it both ways and pick the one that works better.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.