2023-04-24 3:51 AM
according to the reference manual. This can be organized in 1 bank of 2mb or in several banks.
I have created a default project with the stm32cubeide and I would like to know in which mode the flash memory is configured by default. I can't figure out what mode it is in.
Can someone help me with this? Thanks
2023-04-24 6:36 AM
Hello @David Bermúdez,
In STM32CubeIDE, the stm32l4s5xx.h file contains the memory map, the flash memory region should be defined with a starting address and a size.
If flash bank2 macro is not defined then your project contains a single bank
Hope that helps!
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.