2022-01-10 3:36 PM
I've always been curious to know if there was a method to find out the data transferred via the DMA into the peripheral has been sent out probably.
For example a Timer
All it does is
Code:
Create the Array
uint32_t RGB = GREEN << 16 | RED << 8 | BLUE;
wait();
LL_DMA_SetDataLength(DMA1, LL_DMA_STREAM_4, ((offset * 24) + 50));
for (uint32_t LED = 0; LED < offset; LED++) {
if ((offset - 1) == LED) {
for (int bit = 23 + ((int)LED * 24); bit >= 0 + ((int)LED * 24); bit--) {
if ((RGB) & (1 << ((23 + (LED * 24)) - bit))) {
WS28128B_BUFF[bit] = 0xC0;
} else {
WS28128B_BUFF[bit] = 0x60;
}
}
} else {
for (int bit = 23 + ((int)LED * 24); bit >= 0 + ((int)LED * 24); bit--) {
WS28128B_BUFF[bit] = 0x60;
}
}
}
for (uint32_t RESET_LINE = (offset * 24); RESET_LINE < ((offset * 24) + 50); RESET_LINE++) {
WS28128B_BUFF[RESET_LINE] = 0x00;
}Enable DMA and Peripheral
LL_DMA_EnableStream(DMA1, LL_DMA_STREAM_4);
LL_TIM_EnableCounter(TIM15);
WS2812B::block = true;Once DMA Transfer Flag complete flag is done disable
extern "C" void DMA1_Stream4_IRQHandler() {
LL_DMA_ClearFlag_TC4(DMA1);
LL_TIM_DisableCounter(TIM15);
WS2812B::block = false;
}Can I trust the DMA flag, when its set for the data to be sent out to the real world or do I need to now rely on a flag within the TIMER peripheral to do that?
Solved! Go to Solution.
2022-01-10 4:38 PM
The DMA TC flag indicates the data has been transferred to the peripheral, but not that the peripheral is "done" with it. You would need to wait another timer update cycle for this to happen and there's no super clean way of doing it.
An alternative is to add an additional dummy byte at the end of the buffer that doesn't affect the stream (i.e. CCR value for 0% duty cycle) and interrupt during that byte (at the TC flag). Double check on a scope, you may need two dummy bytes.
2022-01-10 4:38 PM
The DMA TC flag indicates the data has been transferred to the peripheral, but not that the peripheral is "done" with it. You would need to wait another timer update cycle for this to happen and there's no super clean way of doing it.
An alternative is to add an additional dummy byte at the end of the buffer that doesn't affect the stream (i.e. CCR value for 0% duty cycle) and interrupt during that byte (at the TC flag). Double check on a scope, you may need two dummy bytes.
2022-01-10 5:08 PM
Is there no more of a definitive way to know if the peripheral is "done"? For example for let say UART, cant really send empty bytes into it like you can with the TIMER.
2022-01-10 5:46 PM
2022-01-10 5:59 PM
Ah I see fair enough, or I guess the "TC" Flag in the UART. Thank you for the explanation
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.