2022-01-12 8:43 PM
I bought hundreds of stm32f427vgt6 MCUs, They work abnormally—— The flash size@ address 0x1FFF 7A22 value is 0xFFFF, In theory it should be 0x0400. The MCU uid @ address 0x1FFF 7A10 of the same batch is irregular,but it should be regular according to previous data.
So, are these MCUs fake ?
Is there any good way to identify whether MCU is genuine or fake ?
Solved! Go to Solution.
2022-01-13 1:15 AM
Welcome, @Ryan Luo, to the community!
Unfortunately, this question has been asked quite often lately. The probability of a fake is very high if the reported flash size and uid are not correct.
Please have a look here and there, maybe it will help you?
Regards
/Peter
2022-01-13 1:15 AM
Welcome, @Ryan Luo, to the community!
Unfortunately, this question has been asked quite often lately. The probability of a fake is very high if the reported flash size and uid are not correct.
Please have a look here and there, maybe it will help you?
Regards
/Peter
2022-01-18 12:33 AM
Thanks for your answer!
I wonder whether the two parameters of flash size and uid can be modified after leaving the factory?
2022-01-18 12:49 AM
No, you can consider these values as OTP (One-Time Programmable), they cannot be changed after leaving the factory.
2022-01-18 5:56 AM
If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.