2017-02-21 7:23 PM
Hi all,
1. I have two question before developing my delay and sum beamforming algorithm.
A). I am working on
Stm32
STM32F401RE NUCLEO with X-NUCLEO-CCA02M1 on Stm32 OsxAcosticBF stack in this source code they are collecting microphone PDM data in to this'I2S_InternalBuffer'
''uint16_t * DataTempI2S = &(I2S_InternalBuffer[X_NUCLEO_CCA02M1_Handler.PdmBufferSize/2]);
uint8_t a,b=0;for(index=0; index<X_NUCLEO_CCA02M1_Handler.PdmBufferSize/2; index++) {a = ((uint8_t *)(DataTempI2S))[(index*2)];b = ((uint8_t *)(DataTempI2S))[(index*2)+1];((uint8_t *)(X_NUCLEO_CCA02M1_Handler.PDM_Data))[(index*2)] = Channel_Demux[a & CHANNEL_DEMUX_MASK] | Channel_Demux[b & CHANNEL_DEMUX_MASK] << 4;;((uint8_t *)(X_NUCLEO_CCA02M1_Handler.PDM_Data))[(index*2)+1] = Channel_Demux[(a>>1) & CHANNEL_DEMUX_MASK] |Channel_Demux[(b>>1) & CHANNEL_DEMUX_MASK] << 4;''after demuxing R/L data they are passed that data into PDM library which is convert R/L data(PDM format ) into PCM format.
here i want to know- that PCM data they are collecting into any buffer or directly they are passed into OsxAcosticBF algorithm library .
B.) how can i use delay between two microphone after getting PCM data because that data in digital format?
regards
vinod
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.