2017-11-16 6:33 PM
HI.
Please help.
CPU : STM32F207
Use the tcp_echoserver example to send and receive data.
#define TCP_MSS 1460, #define TCP_TMR_INTERVAL 250
If data is sent in tcp_echoserver_poll function and the data to send at once is 2000byte,
should I send 540byte after sending 1460byte?
If I'm running the example above, send 1460 bytes and use the tcp_echoserver_poll function A delay of 250ms occurs until it is re-executed. Is there a way to minimize this delay?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.