2024-04-12 10:27 AM
Hi community!
I am working on a hobby project (custom pcb) where i need my stm32 mcu to communicate with a wifi chip, which will send data to a second pcb which is a usb dongle with a similar mcu+wifi setup, only that wifi chip acts as an access point only the first mentioned wifi chip can access and send/receive data from.
How would i go about this and what wifi chip is recommended for it?
I am planning to use the STM32H745IIT6. (maybe a bit overkill, but i need it to process a lot of stuff).
Another thing is that i want to connect 16 small boards, (which contain a BMM350 and a BMI323) to the MCU via I2C, because the STM32H745IIT6 has 4 I2C Interfaces. Is this feasable to do?
I appreciate the assistance.
Thanks,
2024-04-12 12:52 PM
There are wi-fi modules that support both AP and station modes, for example this one is used in some ST eval. boards: MXCHIP EMW3080B. And there are ESP8266 and other ESP chips.
2024-04-13 12:07 AM
Thanks!
I will probably use the ESP8266EX.
Any tips on the second part of the question?
For some more clarification, the STM32H745IIT6 has 4 I2C interfaces i'm using, and it also has 4 SPI interfaces i could use. Would i be better of using The I2C interfaces, the SPI interfaces, or a combination of both?
2024-04-13 1:23 AM
Hi,
1 - ESP8266 is ok (but ESP32-S2-mini : i would think about using it and no H7 , cpu here 32bit/240MHz (almost same power as an H7 ), and 2MB RAM , 4MB flash + SPI, I2C etc... at 2,50 !
https://de.aliexpress.com/item/1005005977413920.html
2 - How long will be connection line to this gyro/magnetic sensors ? screened ?
2024-04-13 5:13 AM
Hi,
1) Thanks for the suggestion! Will definately look into that.
2) Quite long since the 16 sensor packages are individual motion trackers that are relatively far appart
2024-04-13 9:01 AM
I just asked, because in my experience I2C with more than 100mm wire making problems.
Especially with STM CPUs I had no reliable communication.
Much better with SPI here, even at high speed, 16 or 48 Mbit!
Example: I use SPI at 16Mhz to transfer audio data streams from ESP 8266 to H743 CPU over 40cm distance, using a Cat6 network cable.
2024-04-13 9:09 AM
Ah i understand now, thanks for the clarification.
So SPI would be able to handle up to 16 devices (split across 4 SPI interfaces) right?
2024-04-13 9:19 AM
I think we need a much more complete description of your application in order to suggest anything cogent.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.