2017-10-20 5:28 AM
hi,
i wrote Led blink with stm32f103re , and i did write this code :
&sharpinclude 'stm32f10x.h'
&sharpinclude 'delay.h'int main(){ RCC_DeInit ( ) ; RCC_HSEConfig ( RCC_HSE_ON) ; RCC_WaitForHSEStartUp ( ); RCC_PLLConfig ( RCC_PLLSource_HSE_Div1, 9) ; RCC_PLLCmd ( ENABLE ); delay_ms(1); RCC_SYSCLKConfig ( RCC_SYSCLKSource_PLLCLK ); RCC_HCLKConfig ( RCC_SYSCLK_Div1 ); RCC_PCLK2Config ( RCC_HCLK_Div1 ); RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA , ENABLE);GPIO_InitTypeDef gpio; gpio.GPIO_Pin = GPIO_Pin_0; gpio.GPIO_Speed = GPIO_Speed_50MHz; gpio.GPIO_Mode = GPIO_Mode_Out_PP; GPIO_Init(GPIOA , &gpio); while(1) { GPIOA->BSRR = GPIO_Pin_0; delay_ms(300); GPIOA->BSRR = (GPIO_Pin_0<<16); delay_ms(300); }}
But when cpu do delay _ms(300) , the delay is not real , it wait for 3 seconds,
and i modify RCC_ ... register to earn 1 second , but i cant earn that !!
what shall i do to earn real 1 second?I test some ways , but i cant do that yet.
I know that i have problem in RCC setting , but i dont know where!!!
so thanks.#1seconds2017-10-20 6:02 AM
The internal clocks can be output via PA8 (MCO)
Use SysTick to count 1000 milliseconds, or a TIM to count 36 million microseconds.
Better yet, get the TIM to toggle the pin.
Look at example code in system_stm32f1xx.c for how to set up and wait for HSE, PLL, etc.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.