2021-03-22 2:14 AM
when i use the ITCM of stm32h743 with arm gcc ,in linkscript,i add new section as:
_sitcm_addr = LOADADDR(.ItcmRam);
_svtor_addr = LOADADDR(.isr_vector);
_vtor_size = 0x400; /*SIZEOF (.isr_vector)*/
.ItcmRam :
{
. = _vtor_size; /*reserved for vector table*/
. = ALIGN(4);
_sitcm = .; /* create a global symbol at ITCM start */
*(.ItcmRam); /* ram_itcm */
. = ALIGN(4);
_eitcm = .; /* define a global symbol at ITCM end */
} >ITCMRAM AT> FLASH
where ITCMRAM in memory
MEMORY
{
DTCMRAM (xrw) : ORIGIN = 0x20000000, LENGTH = 128K
RAM_D1 (xrw) : ORIGIN = 0x24000000, LENGTH = 512K
RAM_D2 (xrw) : ORIGIN = 0x30000000, LENGTH = 288K
RAM_D3 (xrw) : ORIGIN = 0x38000000, LENGTH = 64K
ITCMRAM (xrw) : ORIGIN = 0x00000000, LENGTH = 64K
FLASH (rx) : ORIGIN = 0x8000000, LENGTH = 2048K
}
in startup file ,i copy .ItcmRam section content from flash to itcm ram after .bss section,like this
CopyItcmInit:
ldr r3, =_sitcm_addr
ldr r3, [r3, r1]
str r3, [r0, r1]
adds r1, r1, #4
LoopCopyItcmInit:
ldr r0, =_sitcm
ldr r3, =_eitcm
adds r2, r0, r1
cmp r2, r3
bcc CopyItcmInit
in source file ,i make some function in ItcmRam section like
void TestItcm(void) __attribute__((section(".ItcmRam"),__long_call__));
in main(){
TestBF();
TestItcm();
TestAF()
}
it works right that can go into the function TestItcm,but no code to run
00000400: movs r0, r0
00000402: movs r0, r0
00000404: movs r0, r0
00000406: movs r0, r0
00000408: movs r0, r0
0000040a: movs r0, r0
0000040c: movs r0, r0
0000040e: movs r0, r0
00000410: movs r0, r0
00000412: movs r0, r0
74 }
in map flie ,i can see
.ItcmRam 0x0000000000000000 0x420 load address 0x00000000080088ac
0x0000000000000400 . = _vtor_size
*fill* 0x0000000000000000 0x400
0x0000000000000400 . = ALIGN (0x4)
0x0000000000000400 _sitcm = .
*(.ItcmRam)
.ItcmRam 0x0000000000000400 0x20 ./Src/main.o
0x0000000000000400 TestItcm
0x0000000000000420 . = ALIGN (0x4)
0x0000000000000420 _eitcm = .
.rel.dyn 0x0000000000000420 0x0 load address 0x0000000008008ccc
.rel.iplt 0x0000000000000420 0x0 /usr/lib/gcc/arm-none-eabi/10.2.0/thumb/v7e-m+dp/hard/crtbegin.o
pc is jumped to itcm at 0x400,but no code in flash address of 0x00000000080088ac
debug like this
080088a9: movs r0, r2
080088ab: movs r0, r0
080088ad: movs r0, r0
080088af: movs r0, r0
080088b1: movs r0, r0
080088b3: movs r0, r0
080088b5: movs r0, r0
080088b7: movs r0, r0
080088b9: movs r0, r0
080088bb: movs r0, r0
080088bd: movs r0, r0
080088bf: movs r0, r0
IS there some method to use stm32h7x's itcm ram with GCC? thanks!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.