2019-11-13 12:19 PM
HI
I am using the STM32L475 IoT discovery kit, I want put my board into deep sleep and wake up every one hour based on event, I was considering setting up alarm clock. I am using x-cube-cld-gen library'r MQTT example.
For now i have scene other examples and set up the alarm sample code. But i don't get the HAL_RTC_AlarmAEventCallback trigger. The clock just keeps on running.
/* Configure the system clock */
SystemClock_Config();
Periph_Config();
BSP_LED_Init(LED_GREEN);
// BSP_PB_Init(BUTTON_USER, BUTTON_MODE_EXTI);
/* RNG init function */
hrng.Instance = RNG;
if (HAL_RNG_Init(&hrng) != HAL_OK)
{
Error_Handler();
}
/* UART console init */
Console_UART_Init();
hrtc.Instance = RTC;
/* RTC init */
RTC_Init();
RTC_AlarmConfig();
#ifdef FIREWALL_MBEDLIB
firewall_init();
#endif
while(1){
RTC_TimeShow(aShowTime);
if(wake_up_time){
printf("I woke up on time....\r\n");
}
HAL_Delay(1000);
}void Periph_Config(void)
{
RCC_PeriphCLKInitTypeDef PeriphClkInit;
PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_RTC|RCC_PERIPHCLK_USART1
|RCC_PERIPHCLK_USART3|RCC_PERIPHCLK_I2C2
|RCC_PERIPHCLK_RNG;
PeriphClkInit.Usart1ClockSelection = RCC_USART1CLKSOURCE_PCLK2;
PeriphClkInit.Usart3ClockSelection = RCC_USART3CLKSOURCE_PCLK1;
PeriphClkInit.I2c2ClockSelection = RCC_I2C2CLKSOURCE_PCLK1;
PeriphClkInit.RngClockSelection = RCC_RNGCLKSOURCE_MSI;
PeriphClkInit.RTCClockSelection = RCC_RTCCLKSOURCE_LSE;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
{
Error_Handler();
}
__HAL_RCC_PWR_CLK_ENABLE();
if (HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1) != HAL_OK)
{
Error_Handler();
}
}static void RTC_Init(void)
{
/**Initialize RTC Only */
hrtc.Instance = RTC;
hrtc.Init.HourFormat = RTC_HOURFORMAT_24;
hrtc.Init.AsynchPrediv = 0x7F;
hrtc.Init.SynchPrediv = 0xF9;
hrtc.Init.OutPut = RTC_OUTPUT_DISABLE;
#ifdef RTC_OUTPUT_REMAP_NONE
hrtc.Init.OutPutRemap = RTC_OUTPUT_REMAP_NONE;
#endif
hrtc.Init.OutPutPolarity = RTC_OUTPUT_POLARITY_HIGH;
hrtc.Init.OutPutType = RTC_OUTPUT_TYPE_OPENDRAIN;
if (HAL_RTC_Init(&hrtc) != HAL_OK)
{
Error_Handler();
}
}static void RTC_AlarmConfig(void)
{
printf("Setting alarm...\r\n");
RTC_DateTypeDef sdatestructure;
RTC_TimeTypeDef stimestructure;
RTC_AlarmTypeDef salarmstructure;
/*##-1- Configure the Date #################################################*/
/* Set Date: Tuesday February 18th 2014 */
sdatestructure.Year = 0x14;
sdatestructure.Month = RTC_MONTH_FEBRUARY;
sdatestructure.Date = 0x18;
sdatestructure.WeekDay = RTC_WEEKDAY_TUESDAY;
if(HAL_RTC_SetDate(&hrtc,&sdatestructure,RTC_FORMAT_BCD) != HAL_OK)
{
/* Initialization Error */
Error_Handler();
}
/*##-2- Configure the Time #################################################*/
/* Set Time: 02:20:00 */
stimestructure.Hours = 0x02;
stimestructure.Minutes = 0x20;
stimestructure.Seconds = 0x00;
stimestructure.TimeFormat = RTC_HOURFORMAT12_AM;
stimestructure.DayLightSaving = RTC_DAYLIGHTSAVING_NONE ;
stimestructure.StoreOperation = RTC_STOREOPERATION_RESET;
if(HAL_RTC_SetTime(&hrtc,&stimestructure,RTC_FORMAT_BCD) != HAL_OK)
{
/* Initialization Error */
Error_Handler();
}
/*##-3- Configure the RTC Alarm peripheral #################################*/
/* Set Alarm to 02:20:30
RTC Alarm Generation: Alarm on Hours, Minutes and Seconds */
salarmstructure.Alarm = RTC_ALARM_A;
salarmstructure.AlarmDateWeekDay = RTC_WEEKDAY_MONDAY;
salarmstructure.AlarmDateWeekDaySel = RTC_ALARMDATEWEEKDAYSEL_WEEKDAY;
salarmstructure.AlarmMask = RTC_ALARMMASK_DATEWEEKDAY;
salarmstructure.AlarmSubSecondMask = RTC_ALARMSUBSECONDMASK_NONE;
salarmstructure.AlarmTime.TimeFormat = RTC_HOURFORMAT12_AM;
salarmstructure.AlarmTime.Hours = 0x02;
salarmstructure.AlarmTime.Minutes = 0x20;
salarmstructure.AlarmTime.Seconds = 0x30;
salarmstructure.AlarmTime.SubSeconds = 0x56;
if(HAL_RTC_SetAlarm_IT(&hrtc,&salarmstructure,RTC_FORMAT_BCD) != HAL_OK)
{
/* Initialization Error */
Error_Handler();
}
}void HAL_RTC_AlarmAEventCallback(RTC_HandleTypeDef *hrtc)
{
/* Turn LED2 on: Alarm generation */
wake_up_time = true;
BSP_LED_On(LED2);
}I was using the STM32L476G-EVAL's RTC_Time project as reference from the stm32cubel4 library samples.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.