2014-03-10 4:15 PM
Hello All,
I'm communicating with a wifi module that uses a stm32 internally and it supports up to 2073600. I can use that baud rate with usb to uart adapter and communicate with the wifi module but when I put my stm32f4 discovery any higher than 921600 it does not seem to work. Is it possible to achieve this speed ? Thanks !void setupCommUart(int baud)
{
USART_InitTypeDef USART_InitStructure;
GPIO_InitTypeDef GPIO_InitStructure;
// init clocks
RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART2,ENABLE);
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE);
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2 | GPIO_Pin_3;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(GPIOA, &GPIO_InitStructure);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource2, GPIO_AF_USART2);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource3, GPIO_AF_USART2);
//110, 150, 300, 1200, 2400, 4800, 9600, 19200, 38400, 57600, 115200, 230400, 460800, 921600
USART_InitStructure.USART_BaudRate = baud;
USART_InitStructure.USART_WordLength = USART_WordLength_8b;
USART_InitStructure.USART_StopBits = USART_StopBits_1;
USART_InitStructure.USART_Parity = USART_Parity_No;
USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;
USART_Init(USART2, &USART_InitStructure);
// enable usart
USART_Cmd(USART2, ENABLE);
}
#discovery #stm32f4 #uart
2015-11-11 4:38 PM
Really not much to go on there. 1200 baud should work. Perhaps you can output a stream of 'U' characters, and scope the output to confirm the bit rate.
Suggest you start a new thread where you present the code, and connectivity.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.