STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Unable to erase Flash sector - STM32F4Discovery

Posted on November 11, 2015 at 17:41I have the following code:  FLASH_EraseInitTypeDef EraseInitStruct;    __HAL_FLASH_INSTRUCTION_CACHE_RESET ();     __HAL_FLASH_INSTRUCTION_CACHE_ENABLE ();     HAL_FLASH_Unlock ();     /* Get the 1st sector to er...

Java just broke

Posted on November 10, 2015 at 20:49And with it broke the STM32CubeMX tool. Probably nothing can be done until Oracle fixes their Java install files.

LMI2 by Lead
  • 1283 Views
  • 3 replies
  • 0 kudos

STM32L0 Discovery + Ammeter

Posted on October 17, 2015 at 12:19I have an STM32L0 DISCOVERY board and I remove the jumper from JP4 and attach my own ammeter between pins 1 and 2.The demonstration software shows between 210uA - 300uA repeatedly but does not execute code.  The LE...

HAL UART Transmit problem

Posted on November 08, 2015 at 21:19I have a running project with STM32F103 and I wanted to add UART Transmit to do some debugging but HAL_UART_Transmit does not work and does not transmit any data. I have chosen USART2 and PD.5 and PD.6 pins as the...

SPI DMA - too much delay time between bytes

Posted on November 11, 2015 at 17:36 Hello there! In my application, I have a 320x240 graphic display (IlI9341 disp dirver), which I'm communicating with on SPI interface; the SPI clock is 10MHz, this is the max supported speed for the di...

Cube Firmware Error in osPoolAlloc function in cmsis_os.c

Posted on July 14, 2015 at 00:42In the latest version of the STM32CubeF4 package (and the last few I've used), there seems to be an error in the CMSIS OS wrapper for FreeRTOS. I imagine this is in the other Cube packages as well, though I haven't lo...

CAN FILTERS

Posted on November 11, 2015 at 17:48 Hi every one, especially Mr.Clive, today i have problem with CAN FILTERS i want to allow all IDS from 100 to 1FF in other words block all messages after 0x0200 here is my code, Please help me, Thanks in ad...

puneethj by Associate II
  • 1421 Views
  • 1 replies
  • 0 kudos

Connect two timers in Gated Mode

Posted on November 10, 2015 at 09:42Hi, unfortunately I haven't understood how to connect two timers. I want to achieve a 3,2kHz PWM switch signal that turns on and off a 1 MHz signal. I try to setup TIM3 as a master timer; in STM32CubeMX I have sel...

smrtkai by Senior
  • 2288 Views
  • 4 replies
  • 0 kudos

stm32f4 Timer

Posted on November 10, 2015 at 17:34Hello every one! How can i check if the timer is already running.. which flag to use I am trying thisif (TIM2 -> CR1 == TIM_CR1_CEN){// turn led on blue} else{// turn led red on}but it does not work, please help m...

puneethj by Associate II
  • 1959 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.