2018-11-03 1:41 PM
2018-11-03 1:41 PM
Does Suresh have a question?
2018-11-03 1:45 PM
yes. I cant use my stlink and blue pill module, STM32F103C8 (Blue PILL) and STM32F103CB6T(STLINK clone). Driver not properly not installed and also I cant debug and flash my target board.
I got below error
Target not found,
2018-11-03 1:49 PM
Target core not powered.
SWDIO/SWCLK not correctly connected.
ST-LINK not connected to VTarget and GND.
2018-11-03 1:51 PM
3.3 to 3.3
gnd to gnd
swio to io
clk to clk
2018-11-03 1:52 PM
this is forum also looking great like arduino
2018-11-03 1:53 PM
thanks for buddy for replying
2018-11-03 1:53 PM
in india the time is 2:23 AM
2018-11-03 5:29 PM
And you've measured 3 or 3.3V ?
I'm not using blue pill boards, if it has a USB port you could try pulling the BOOT0 pin high and seeing if will connect in DFU mode. If so you could use the Cube STM32 Programmer application.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.