2021-06-30 8:24 AM
2021-06-30 8:49 AM
What FLASH?
JW
2021-06-30 8:58 AM
A "file" is quite a complex concept. What kind of file do you mean?
2021-06-30 9:08 AM
STM32Cube_FW_L4_V1.16.0\Projects\32L4R9IDISCOVERY\Applications\FatFs\FatFs_uSD_Standalone ??
STM32Cube_FW_L4_V1.16.0\Projects\32L496GDISCOVERY\Examples\FLASH\FLASH_EraseProgram
STM32Cube_FW_L4_V1.16.0\Projects\32L496GDISCOVERY\Examples\FLASH\FLASH_FastProgram
Internal Flash, probably no, its not how people generally approach the problem.
You can create resource trees, or file system type structures, and put them in memory permanently, perhaps wrapping them with file system type access functions to make porting easier.
Perhaps look at MKFSDATA type tools used by LWIP, or similar tools, to create a faux web server
If needing an actual file system, perhap FATFS onto MicroSD cards, or eMMC chips.
Can be done with QSPI NOR Flash, or NAND/NOR Flash generally, but you get to own a lot more of the fine details.
2021-06-30 9:11 AM
txt file
2021-06-30 9:56 AM
Just one, of manageable size, perhaps carve some space in the upper reach of the internal flash sectors, store the data, provide means to erase/write new content.
2021-07-05 5:29 AM
Yes a want a small txt file in the internal flash, thanks.
Where can I find any examples? please
2021-07-05 5:30 AM
I am using the B-L4s5I-IOT01A board
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.