STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

TIMx Link TIMX to Measure External Frequency

Am using NUCLEO-STM32H723 Nucleo-144 board.Sorry, but I have no experience with the above MCU/TIMx.My goal is to measure external frequency as accurately as possible.I'm interested to know how to Link between two timers.Example : TIM3 ( Master ) TI...

0693W00000BclHJQAZ.jpg 0693W00000BclG2QAJ.jpg
ESega.1 by Associate II
  • 4361 Views
  • 9 replies
  • 0 kudos

I need to configure CAN filters in such a way that only ID 0x80 and IDs between 0x200 and 0x300 passes all others are not allowed to be passed. How to do that?

I tried in this way but the problem is only 200-300 can pass but 80h is not passed. if i use if else then only 80h is passed not 200-300h. So, the problem is i can pass either 80h or 200h-300h. Not both 80h and 200-300h. #define Filter_ID1  0x80#def...

MAlam.2 by Associate II
  • 3140 Views
  • 6 replies
  • 1 kudos

STM32L552ZE-Q SAI I2S slave pass data to master output

My development board is STM32L552ZE-Q.I want to use SAI slave mode receive i2s signal and SAI master transmit i2s signal.I can observe clock and makesure data in have input.But my data out isn't similar with my input.Does any one can help me, thanks

CTsai.1 by Associate
  • 700 Views
  • 0 replies
  • 0 kudos

SPI TXEIE is not SET even after configured it

I have done some debugging on SPI interrupt problem. So, I have a function that SPI_SendDataIT which means SPI send data with interrupt. the interrupt will be triggered if TXE flag is SET. But we have to enable the TXEIE first. But, what happen is, a...

0693W00000BckgSQAR.png 0693W00000BckgIQAR.png
WM_IR by Senior
  • 3262 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.