2020-08-25 9:15 AM
Here is the RTC initialization code:
static void MX_RTC_Init(void)
{
/* USER CODE BEGIN RTC_Init 0 */
/* USER CODE END RTC_Init 0 */
RTC_TimeTypeDef sTime = {0};
RTC_DateTypeDef sDate = {0};
/* USER CODE BEGIN RTC_Init 1 */
/* USER CODE END RTC_Init 1 */
/** Initialize RTC Only
*/
hrtc.Instance = RTC;
hrtc.Init.HourFormat = RTC_HOURFORMAT_24;
hrtc.Init.AsynchPrediv = 127;
hrtc.Init.SynchPrediv = 255;
hrtc.Init.OutPut = RTC_OUTPUT_DISABLE;
hrtc.Init.OutPutPolarity = RTC_OUTPUT_POLARITY_HIGH;
hrtc.Init.OutPutType = RTC_OUTPUT_TYPE_OPENDRAIN;
if (HAL_RTC_Init(&hrtc) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN Check_RTC_BKUP */
/* USER CODE END Check_RTC_BKUP */
/** Initialize RTC and set the Time and Date
*/
sTime.Hours = 0x15;
sTime.Minutes = 0x00;
sTime.Seconds = 0x00;
sTime.DayLightSaving = RTC_DAYLIGHTSAVING_NONE;
sTime.StoreOperation = RTC_STOREOPERATION_RESET;
if (HAL_RTC_SetTime(&hrtc, &sTime, RTC_FORMAT_BCD) != HAL_OK)
{
Error_Handler();
}
sDate.WeekDay = RTC_WEEKDAY_THURSDAY;
sDate.Month = RTC_MONTH_AUGUST;
sDate.Date = 0x8;
sDate.Year = 0x1985;
if (HAL_RTC_SetDate(&hrtc, &sDate, RTC_FORMAT_BCD) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN RTC_Init 2 */
/* USER CODE END RTC_Init 2 */
}
In main function I just have a loop that reads date, time, and prints time to the serial port.
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
RTC_TimeTypeDef Time_Stamp;
RTC_DateTypeDef sDate;
HAL_RTC_GetDate(&hrtc,&sDate,RTC_FORMAT_BIN );
HAL_RTC_GetTime(&hrtc,&Time_Stamp,RTC_FORMAT_BIN);
sprintf(str,"%d:%d:%d:%d",Time_Stamp.Hours,Time_Stamp.Minutes,Time_Stamp.Seconds,Time_Stamp.SubSeconds);
HAL_UART_Transmit_DMA(&huart2,&str,15);
HAL_Delay(1000);
}
The RTC clock input is set to LSE in system clock config:
PeriphClkInit.RTCClockSelection = RCC_RTCCLKSOURCE_LSE;
Here is what I get from serial port:
15:0:0:255
15:0:0:0
15:0:1:0
15:0:1:0
15:0:1:0
15:0:1:0
15:0:1:1
15:0:1:1
15:0:1:1
15:0:1:1
15:0:1:1
15:0:1:1
15:0:1:2
15:0:1:2
15:0:1:2
15:0:14:2
15:0:14:2
15:0:14:2
15:0:14:2
15:0:14:3
15:0:14:3
15:0:14:3
15:0:14:3
15:0:14:3
15:0:14:4
15:0:14:4
15:0:14:4
15:0:26:4
15:0:26:4
15:0:26:4
15:0:26:5
15:0:26:5
15:0:26:5
15:0:26:5
15:0:26:5
15:0:26:5
15:0:26:5
15:0:26:6
15:0:26:6
15:0:38:6
15:0:38:6
15:0:38:6
15:0:38:6
15:0:38:7
15:0:43:7
15:0:43:7
15:0:45:7
15:0:45:7
15:0:45:7
15:0:45:8
15:0:45:8
15:0:50:8
15:0:50:8
15:0:50:8
15:0:53:8
15:0:53:9
15:0:53:9
15:0:53:9
15:0:57:9
15:0:57:9
15:0:57:9
15:0:57:9
15:0:57:10
15:0:57:10
15:0:57:10
15:1:4:10
15:1:4:10
15:1:4:10
15:1:7:11
15:1:7:11
15:1:7:11
15:1:7:11
15:1:7:11
15:1:7:11
15:1:7:12
15:1:14:12
15:1:14:12
15:1:14:12
15:1:14:12
15:1:14:12
15:1:14:13
15:1:14:13
15:1:14:13
15:1:22:13
15:1:22:13
15:1:22:13
15:1:22:14
15:1:22:14
15:1:27:14
15:1:27:14
Also note it printed more that 60 times before the minutes value updated from 0 to 1 minute... I know the delay function is not 100% accurate for measuring time but it shouldnt have such huge deviation. If I leave it running the minutes continue to increase but compared to my PC clock they have deviation if I leave it for 30 minutes or so.. The prediv values are correct for 32.768Khz clock:
hrtc.Init.AsynchPrediv = 127;
hrtc.Init.SynchPrediv = 255;
Any help would be highly apreciated. Thanx
Solved! Go to Solution.
2020-08-25 11:36 AM
2020-08-25 10:41 AM
You're using BCD not binary 0x09 ticks to 0x10, 0x49 to 0x50, and 0x59 to 0x00
uint8_t str[32];
HAL_UART_Transmit_DMA(&huart2, &str, sprintf((char *)str,"%02d:%02d:%02d:%d\n",Time_Stamp.Hours,Time_Stamp.Minutes,Time_Stamp.Seconds,Time_Stamp.SubSeconds));
sprintf returns length of string
2020-08-25 11:36 AM
First read time, then date.
JW
2020-08-26 2:01 AM
waclawek.jan thank you. it works now!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.