2021-07-24 1:54 AM
the errors like :\st\stm32cubeide_1.6.1\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_1.5.0.202011040924\tools\arm-none-eabi\bin\ld.exe: STM32F469I-DISCO.elf section `ExtFlashSection' will not fit in region `QSPI'
c:\st\stm32cubeide_1.6.1\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_1.5.0.202011040924\tools\arm-none-eabi\bin\ld.exe: region `QSPI' overflowed by 887220 bytes
collect2.exe: error: ld returned 1 exit status
make: *** [makefile:92: STM32F469I-DISCO.elf] Error 1
"make -j4 all" terminated with exit code 2. Build might be incomplete.
i checked my liker file
MEMORY
{
CCMRAM (xrw) : ORIGIN = 0x10000000, LENGTH = 64K
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 320K
FLASH (rx) : ORIGIN = 0x8000000, LENGTH = 2048K
SDRAM (rw) : ORIGIN = 0xC0000000, LENGTH = 16M
QSPI (r) : ORIGIN = 0x90000000, LENGTH = 16M
}
in hardware changes also - middleware - free RTOS - advanced settings - enabled USE_NEWLIB_REENTRANT parameter.
i am new to this i couldn't get rid of this .. ..help meeeee
2021-07-24 8:33 AM
PNG size need be same as display and too check if in images you realy have only two images. All too unused images is compiled in code...
2021-07-25 4:07 AM
24MB won't fit in 16MB, check how large these images are and how much of the kitchen is being added.
Could perhaps say QSPI is 32 MB so linker gets closure and then look at what's in the .MAP file.
2021-07-25 7:52 AM
same screens using another project, i didn't get any errors over there
2021-07-26 8:37 AM
Check or show here folder list for TouchGFX\assets\images\ and TouchGFX\generated\images\src\
Directory of ....assets\images
26. 07. 2021 17:35 <DIR> .
26. 07. 2021 17:35 <DIR> ..
18. 10. 2019 15:14 1 079 gauge_needle_pin.png
10. 12. 2019 12:25 140 green1.png
30. 01. 2020 12:26 21 519 Nu-44_L.png
30. 01. 2020 12:26 21 534 Nu-44_R.png
30. 01. 2020 12:26 1 656 Nu-44_S.png
31. 01. 2020 09:24 20 512 Nu-46B_oL.png
31. 01. 2020 09:24 20 581 Nu-46B_oR.png
31. 01. 2020 10:01 1 784 Nu-46B_oS.png
07. 02. 2020 11:04 18 489 ST_103.png
07. 02. 2020 11:04 18 418 vumeter02.png
26. 07. 2021 17:35 <DIR> __designermy example
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.