2022-01-11 12:47 AM
/*CODE to generate PWM signal of 50%*/
#include "stm32l476xx.h"
#include "pwm.h"
void pwm_init(void){
/*RCC configuration*/
RCC->AHB2ENR|=RCC_AHB2ENR_GPIOEEN;//ENABLE GPIOE
RCC->APB2ENR|=RCC_APB2ENR_TIM1EN;// ENABLE CLOCK ACCESS TO TIM1
//RCC->APB1ENR1|=RCC_APB1ENR1_PWREN;// ENABLE POWER INTERFACE CLOCK
/*GPIO configuration*/
GPIOE->MODER &= (~(1U<<16)); // GPIOE selected as alternate function mode
GPIOE->MODER |= (1U<<17);
//GPIOE->MODER|=GPIO_MODER_MODE8; // GPIOE selected as analog function
//GPIOE->ODR|=(1U<<8);
//GPIOE->IDR|=(1U<<8);
GPIOE->AFR[1]|=(1U<<0);
/*Timer configuration*/
TIM1->PSC=0; //set prescalar to 0
TIM1->ARR=8000-1; // auto reload register
TIM1->SR |= (1U<<0)|(1U<<1)|(1U<<2)|(1U<<3)|(1U<<4);
TIM1->BDTR|=(1U<<13);
TIM1->BDTR|=(1U<<15);
TIM1->DMAR|= (0X01U);
TIM1->CCMR1|=(1U<<5);/* Output compare 1 mode as PWM MODE 1*/
TIM1->CCMR1|=(1U<<6);/* Output compare 1 mode as PWM MODE 1*/
// TIM1->CCMR1|=(1U<<4);/* Output compare 1 mode as PWM MODE 1*/
//TIM1->CCMR1|=(1U<<5);/* Output compare 1 mode as PWM MODE 1*/
//TIM1->CCMR1|=(1U<<1);/*output compare preload enable*/
TIM1->CCR1|=(0X0U);//Capture compare register*/
TIM1->CCER|=(1U<<2); // Enable compare
//TIM1->CCER|=(1U<<0);//Enable CH1 compare mode*/
TIM1->CNT=0; // count register
TIM1->CR1|=(1U<<0); // enable timer1
}
Kindly help regarding this....
2022-01-11 1:43 AM
USE MX generated HAL code and learn or examples from folder..., after 10 years you can try start prog with registers...
In your code is big amount of errors
2022-01-11 1:51 AM
Hi,
Thanks for your feed back....
But it was needed to write in register level,so I requested
2022-01-11 3:34 AM
> TIM1->CCR1|=(0X0U);//Capture compare register*/
You need to set CCR1 to ARR/2 to have 50% PWM.
If it still does not work, read out and check/post content of TIM and relevant GPIO registers.
JW
PS. To set individual bits or even bitfields, it's better to use symbols from the CMSIS-mandated device header, e.g.
TIM1->CR1 |= TIM_CR1_CEN; // enable timer 1
PS2.
TIM1->BDTR|=(1U<<13);
this sets TIMx_BDTR.BKP, break polarity, but this is ignored as you don't set break enable, BKE. But setting it opens other ways why the TIM output might not work, so just leave it for now as it is.
2022-01-11 3:46 AM
Waclawek.jan Thank you and thanks for your time and patience.....
2022-01-11 8:31 AM
Note that this is not really PWM - it is just a fixed duty-cycle square wave.
PWM = Pulse Width Modulation, which means that the pulse-width is being modulated - ie, changed.
So a fixed duty-cycle square wave isn't really PWM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.