2021-08-03 3:36 PM
I'm using stm32f429 Discovery board and I want to know number of cycles required to execute this part of assembly code .
ldr r3, [pc, #64] ; (0x8001228 <TIM1_UP_TIM10_IRQHandler+120>)
ldr r3, [r3, #0]
ldr r3, [r3, #36] ; 0x24
ldr r2, [pc, #64] ; (0x800122c <TIM1_UP_TIM10_IRQHandler+124>)
ldr r2, [r2, #0]
subs r2, r3, r2
ldr r3, [pc, #52] ; (0x8001228 <TIM1_UP_TIM10_IRQHandler+120>)
ldr r3, [r3, #0]
subs r2, #25
str r2, [r3, #36] ; 0x24
this assembly code is equivalent to
htim1.Instance->CNT = htim1.Instance->CNT - q - 25 ;
where q is integer number calculated from another expression.
Thanks....
2021-08-03 4:23 PM
You can see the number of cycles per instruction here:
https://developer.arm.com/documentation/ddi0439/b/CHDDIGAC
Note that this doesn't include delays due to accessing, such as flash wait states or bus contention issues.
You can use the DWT->CYCCNT counter to measure things, though you need to initialize it first.
CoreDebug->DEMCR |= CoreDebug_DEMCR_TRCENA_Msk;
DWT->CTRL |= DWT_CTRL_CYCCNTENA_Msk;
DWT->CYCCNT = 0;
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.