2023-01-27 8:41 AM
Have a problem with write Scatter-Loading Description File for STM32H743 (arm keil).
I need to map SDRAM memory.
Regular I do it like:
RW_RAM1 0xD0000000 0x00800000 { ; fmc bank 2
*(SDRAM)
}
On all other MCU's it's work perfect, but not for stm32H7.
It's fail on BX R0 command from startup file:
LDR R0, =SystemInit
BLX R0
LDR R0, =__main
BX R0 //after this command
Solved! Go to Solution.
2023-02-08 8:40 AM
Hello @AOrlo.2,
I guess there is a point missing here
uint16_t bufersdram[10] __attribute__ ((section(".SDRAM")));
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-02-08 10:21 AM
Why?
If I use point like (".SDRAM"), so compiler don't see this section and put it to 0x24000000
If I don't use point ("SDRAM"), I see that it maped to 0xD0000000.
2023-02-08 10:38 AM
@AOrlo.2 Are you using a customized Hardware setup or ST's Board? If possible, please attach binary file.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-02-08 10:45 AM
Use Waveshare CoreH7XXI
2023-02-08 10:48 AM
I have compleatly workable project on CoreF7XXI
But problem that CoreF7XXI no more in stock..
So I try to convers it to H7.
2023-09-26 9:18 PM
@AOrlo.2 Any solution you found? I am also facing similar issue.
2024-10-18 8:36 AM
I met exactly the same problem. By step-in to __main assembly, found the reason is that, __scatterload is trying to copy variables from load address to exec address, which include copy to external SDRAM (0xd0000000), but at this time, external SDRAM not initialized yet, this caused hard fault.
Unfortunately with ARM compiler, unable to find a way to solve this. Looks need ARM support
2024-10-18 8:49 AM
@ukzw wrote:
I met exactly the same problem. By step-in to __main assembly, found the reason is that, __scatterload is trying to copy variables from load address to exec address, which include copy to external SDRAM (0xd0000000), but at this time, external SDRAM not initialized yet, this caused hard fault.
You need that SDRAM is initialized before calling the main() otherwise you will fall in Hardfault.
You can refer to the X-CUBE-H7-PERF
and see how the scatter file under: Projects\STM32H743I_EVAL\stm32h7x3_cpu_perf\MDK-ARM\scatter_file\6-M7-ITCM_rwExtSDRAM.sct
and the SDRAM is configured in SystemInit_ExtMemCtl() in system_stm32h7xx.c are made: need to activate the definition of DATA_IN_ExtSDRAM
And becarefull if you are trying to execute from 0xD0000000, you will fall also in a fault as that region is Execute-Never as described by ARM. So you need to disable it with MPU.
2024-10-18 11:09 AM
>> Looks need ARM support
As I said originally in the thread, the SDRAM needs to be initialized in SystemInit(), this is ** ARM'S ** expectation, it is the contract with you, so that the scatter loader can unpack into viable memory.
Initialize the clocks, pins and peripherals in SystemInit(), doing it in main() is far to late.
2024-10-24 8:40 AM
Thanks SofLit pointing me to X-CUBE-H7-PERF, problem solved!
However I have a few comments wish someday ST/ARM can consider.
I only need store some user data into SDRAM, a simple flag such as "NOLOAD" - maybe GCC have this - shall be easily meet this requirement. I appreciate ARM has reasons to request SDRAM initialization before the main(), but this makes things complicated. system_stm32xx.c is a system file auto-generated, we write application code can expect just use it without need change inside, now I have to add my own code inside this file, which can make future software maintenance difficult.
Also the added code is to directly change the registers - a lot of "magic numbers" makes code difficult to understand. I use H757 with a 16bit width SDRAM, not the same as X-CUBE-H7-PERF which use H743 with a 32bit width SDRAM, so have to do some changes at the register level, this is not very nice code.
If use a flag such as "NOLOAD" to allow running to main() without go to hard fault, then we can initialize SDRAM by use HAL, the code can be much clean and easy to maintain.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.