2020-01-23 12:46 PM
STM32F769I-DISCO offers a part to get it compatible with the RP MIPI DSI 7" Screen (B-LCDAD-RPI1) but there is no firmware support from either company. Does anyone have any information on how to get the two compatible? and if not, is there any other suggestions to upgrading the 4" DSI screen to a different 7" screen that would be much easier to use? Our search so far has been unsuccessful.
Any help at all would be appreciated, Thank You!
2020-05-08 3:23 AM
@CLued.1916 Have you succeeded? I think the main part of the problem is Raspberry Pi is NOT open source and some secrets are keeps particularly well.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.