2013-03-31 11:24 AM
GPIOA_Pin15 connected to CLK
while(GPIOA->IDR <
32765
); // wait if CLK is low,
while(GPIOA->IDR > 32765); // wait if CLK is high, when i go out from this loop CLK should be low
Delay(6); // wait a bit, it is 6x ''nop''
GPIOA->BSRRL= GPIO_Pin_10; // Set Si high
Delay(6); // wait a bit
GPIOA->BSRRH= GPIO_Pin_10; //Set SI low Can i do it by using STM32F4 hardware ? (now stm32f4 core is clocked to 255MHz)
2013-04-01 4:40 PM
Polling is not a good option when you use microcontrollers.
The best option is to use specific timer features. STM32F4 supports input capture, output compare, PWM generation and one-pulse mode output. The STM32F4 timers have up to 11.8ns resolution (AHB/APB1 prescaler distinct from 1, fTIMxCLK=84MHz). Unfortunatetly the datasheet (v3) does not have the timing specifications for the I/O ports. Such timer features allow even slow frameworks (arduino, .netmf) to create or read fast signals. About my other notice, overclocking, the problem is not heat itself but electromigration. Even if the chips' temperature is not above its' specs temparature limit, overclocking rises it's temperature and it reduces the MCU lifetime in long term. http://en.wikipedia.org/wiki/Electromigration2013-04-02 7:54 AM
ok, after long surfing i found why my code is slow.
as it turns out, FIFO Load clock is 8MHz, unload clock with some two floating MAC operation is 7.999MHz, that means that mcu is fast as it can be for this task. but biggest lag is float to integer conversionwhile(1)
{
while(GPIOA->IDR <
32766
);
GPIOD->BSRRL= GPIO_Pin_13;
while(GPIOA->IDR > 32766);
while(GPIOA->IDR <
32766
);
GPIOD->BSRRH= GPIO_Pin_13;
imag=0;
real=0;
i=0;
while(i<
128
)
{
while(GPIOC->IDR <
32766
);
CLK_LOW;
CLK_HIGH;
k
=
GPIOB
->IDR;
real+=k*cosinusas[i];
imag-=k*sinusas[i];
i++;
}
faze=faze-(0.2*Phase(imag,real));
DAC_DATA=(int)(faze*375+32767);
} if i don't use
DAC_DATA=(int)(faze*375+32767); loop speed is 58KHz, if i add DAC_DATA line, speed goes down to 40KHz, why ?
How can i get it done faster ?
DAC_DATA for integer is as fast as FSMC,it don't slow loop at all.
any workaround for this problem ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.