2009-10-28 3:48 AM
HardFault error when accessing DMA configuration-bits using bitbanding
2011-05-17 4:27 AM
Good morning,
I have a somewhat weird problem that is easy to reproduce, but I don't get the reason for it:Code:
int main() { FLASH->ACR = 0x00000012; stm32_ClockSetup(); //Nothing fancy, HSE on, PLL on... BITACCESS(RCC->AHBENR)[0]=1; //DMA clock enable DMA->CPAR3=0xAA5500FF; //Some random address values DMA->CCMAR3=0x000AA000; DMA->CNDTR3=0x05; DMA->CCR3=0x00; DMA->CCR3|=0x02; //Set Bit 1 DMA->CCR3|=0x01; //Set Bit 0 } when I replace either of the last two lines using my BitBanding - Macro (BITACCESS(DMA->CCR3)[1]=1; or BITACCESS(DMA->CCR3)[0]=1; like used before to set DMA clock in RCC), I run into a hard fault error. Using the Keil simulator I can see in the DMA peripheral tab that the correct bits are set. But on the real hardware, hard fault every time. The calculated bit addresses are correct, I checked that. Did I miss something here? Can't I access these bits using bit banding? And why? Regards Benjamin2011-05-17 4:27 AM
1. make sure you enable clock to (both) DMA units
2. make sure the address calculated with your macro is correct 3. btw. the DMA variable is initialized? Hard fault is a generic collector for other exceptions, enable bus fault, usage and memory fault exceptions and read the source instruction address and reason in NVIC error registers. [ This message was edited by: edison on 28-10-2009 16:19 ]We’re moving the ST Community to a new platform to give you a better and more reliable community experience.