2010-04-03 3:48 AM
Hard Real Time contraints on STM32
2011-05-17 4:45 AM
The NVIC is for interrupts. I suppose you could write tasks as interrupts.
Best idea: serious realtime response is ISR. All else is interruptible. Tell us what you are trying to accomplish and perhaps someone will be kind enough to suggest a workable design. Do you need a realtime OS? Post contact info & I will describe a simple non-preemptive multitasking scheduler. (FWIW I live in Santa Clara, CA)2011-05-17 4:45 AM
2011-05-17 4:45 AM
in compiling, i have found the following message in infinite loop ''Usage fault: attempt to use a coprocessor instruction''.
wheras, ''coprocessor instructions are not supported on the Cortex-M3.'' and I've not used any coprpocessor instruction'' definitive guide of cortex-M3. (that's just a migration from an old firmware v0.2 to the newest one v3.2)
here, the code causing compiler message:
/* stm32f10x_it.c */
/***********extern functions declaration****************/
extern void vPortSVCHandler ( void );
/*------------------------------------------------------------*/
void SVC_Handler(void)
{
vPortSVCHandler ();
}
/* portasm.s */
vPortSVCHandler;
ldr r3, =pxCurrentTCB
ldr r1, [r3]
ldr r0, [r1]
ldmia r0!, {r4-r11}
msr psp, r0
mov r0, #0
msr basepri, r0
orr r14, r14, #13
bx r14
--> after the instruction ( bx r14 ), debugger go to SVC_Handler, the massage ''Usage fault: attempt to use a coprocessor instruction'' appear and it makes a HardFault, accessing to the following function:
/* stm32f10x_it.c */
void HardFault_Handler(void)
{
/* Go to infinite loop when Hard Fault exception occurs */
while (1)
{}
}
how can I proceed?
regards
Slim
2011-05-17 4:45 AM
Thanks Anis,
it's all right with stm32f103b.
Slim
2011-05-17 4:45 AM
You can't call down like this. SVC_Handler(void) -> vPortSVCHandler ();
The function vPortSVCHandle must be called directly from the Cortex-M3 vectors. R14 contains a ''magic'' number at that point, not a regular return address. By calling the subroutine, the return address in (LR or R14) points to the instruction after the call, and by modifying you end up executing bad code upon return, and not changing the processor mode. -Clive2011-05-17 4:45 AM
I don't see why vPortSVCHandler shouldn't be called in SVC_Handler. For me it's working fine this way. (see my project attached in my previous post).
It works due to luck and a failure to understand what is being done with R14/LR, and what compilers do with the code. You should see the problem if you look at the code generated. The IAR compiler creates (Your working system, from your compiled ELF object) 08004390 <SVC_Handler>: 8004390: f000 b8fa b.w 8004588 <vPortSVCHandler> 08004588 <vPortSVCHandler>: 8004588: 4b09 ldr r3, [pc, #36] (80045b0 <_?0>) 800458a: 6819 ldr r1, [r3, #0] 800458c: 6808 ldr r0, [r1, #0] 800458e: e8b0 0ff0 ldmia.w r0!, {r4, r5, r6, r7, r8, r9, sl, fp} 8004592: f380 8809 msr PSP, r0 8004596: f04f 0000 mov.w r0, #0 ; 0x0 800459a: f380 8811 msr BASEPRI, r0 800459e: f04e 0e0d orr.w lr, lr, #13 ; 0xd 80045a2: 4770 bx lr Where as Keil uVision3 creates this 08000c4a <SVCHandler>: 8000c4a: b510 push {r4, lr} 8000c4c: f7ff fa58 bl 8000100 <vPortSVCHandler> 8000c50: bd10 pop {r4, pc} 08000100 <vPortSVCHandler>: 8000100: 4ba2 ldr r3, [pc, #648] (800038c <Test_Alert+0x3c>) 8000102: 6819 ldr r1, [r3, #0] 8000104: 6808 ldr r0, [r1, #0] 8000106: e8b0 0ff0 ldmia.w r0!, {r4, r5, r6, r7, r8, r9, sl, fp} 800010a: f380 8809 msr PSP, r0 800010e: f04f 0000 mov.w r0, #0 ; 0x0 8000112: f380 8811 msr BASEPRI, r0 8000116: f04e 0e0d orr.w lr, lr, #13 ; 0xd 800011a: 4770 bx lr In Keil an extra level of abstraction, as defined by your code, will cause an issue. The vPortSVCHandler code needs to be called directly. Even in IAR which has optimized this to a branch you could save time by calling it directly. Try turning off optimization in IAR, things will probably break there too. -Clive
2011-05-17 4:45 AM
From my scheduler:
goTask ldr r1,=curTask str r0,[r1] ;save TT adrs of task we fire up ldr r0,[r0,#TTSP] ldmia r0!,{r4-r11} msr PSP,r0 mov r2,#0xFFFFFFFD ;magic int rtn flag bx r2 Hopefully my spaces remain intact. Calls to my scheduler are via SVC. (Which I had to make the lowest priority but that’s another story.) The above is how I leave the scheduler and fire up a task. Hope this helps.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.