2015-10-21 10:20 AM
Hi,
I am using STM32F746.It is connected with ST wifi module(SPWF01SC) via UART./* Buffer used for transmission */uint8_t aTxBuffer[] = ''AT+S.SOCKD=8825\r\n'';/* Buffer used for reception */uint8_t aRxBuffer[RXBUFFERSIZE];In the program I am using HAL_UART_Transmit_DMA to transfer and HAL_UART_Receive_DMA to receive.I am transmitting the buffer to start the wifi module and it is working fine.Now I am sending a string ''PIP'' from my wifi module.whenever I receive this string''PIP'' the MCU need to transmit back ''CIAO''.In my case I am receiving the string CIAO only when I reset the MCU and also it is working fine only for the first time after reset then for the second time i need to send the string twice then i get the response but after that there is no response.my main loop code : UartHandle.Instance = USARTx; UartHandle.Init.BaudRate = 115200; UartHandle.Init.WordLength = UART_WORDLENGTH_8B; UartHandle.Init.StopBits = UART_STOPBITS_1; UartHandle.Init.Parity = UART_PARITY_NONE; UartHandle.Init.HwFlowCtl = UART_HWCONTROL_NONE; UartHandle.Init.Mode = UART_MODE_TX_RX; if(HAL_UART_DeInit(&UartHandle) != HAL_OK) { Error_Handler(); } if(HAL_UART_Init(&UartHandle) != HAL_OK) { Error_Handler(); } if(HAL_UART_Transmit_DMA(&UartHandle, (uint8_t*)aTxBuffer, TXBUFFERSIZE)!= HAL_OK) { Error_Handler(); } /*##-3- Wait for the end of the transfer ###################################*/ while (UartReady != SET) { } while (1) { HAL_Delay(100); if(HAL_UART_Receive_DMA(&UartHandle, (uint8_t *)aRxBuffer, RXBUFFERSIZE) != HAL_OK) { // Error_Handler(); } if(aRxBuffer[0]=='P'&&aRxBuffer[1]=='I'&&aRxBuffer[2]=='P') { aTxBuffer[0]='C'; aTxBuffer[1]='I'; aTxBuffer[2]='A'; aTxBuffer[3]='O'; aTxBuffer[4]='\r'; aTxBuffer[5]='\n'; BSP_LED_On(LED1); txBuf = 5; if(HAL_UART_DeInit(&UartHandle) != HAL_OK) { Error_Handler(); } if(HAL_UART_Init(&UartHandle) != HAL_OK) { Error_Handler(); } if(HAL_UART_Transmit_DMA(&UartHandle, (uint8_t*)aTxBuffer, txBuf)!= HAL_OK) { //Error_Handler(); } while (UartReady != SET) { } aRxBuffer[0]='a'; } }Help me guys with some solution.my MCU need to reply back CIAO whenever I receive PIP on the UART.Please have a look at the image.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.