STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Stop PWM output after N steps

Posted on August 27, 2012 at 20:01Is there a way to tell a TIMer on STM32 chips to do some number of steps and automatically stop after finished (and give an interrupt)?  I can do it now with a counter in the ISR but a few pulses slip out before I c...

Precise frequency measurement with STM32F3

Posted on October 20, 2015 at 15:51Hi, all. Could you please recommend the best way to do that using STM32 Timers? Input signal is a 5-10 kHz 3V sine-wave, and high-stable TCXO 12 MHz is used for MCU clocking. Measurement should be done with 1E-3 H...

krdmitry by Associate II
  • 4679 Views
  • 6 replies
  • 0 kudos

STM32F373 - Strange sigma-delta AD behaviour

Posted on October 21, 2015 at 21:21My colleague uses STM32F373 and he found a strange behaviour with SD AD. Actually, this behaviour is described in ref. manual, but I am just curious why it is like that...He starts SD AD conversion with software co...

matic by Associate III
  • 1249 Views
  • 2 replies
  • 0 kudos

STM32L0x1 Accurate LSE Clocks

Posted on October 21, 2015 at 17:40Hello! We are trying to generate a clock signal around 1.024MHz.  We currently have a 32768 watch crystal connected up and are hoping to get at least the 0.5% accuracy as alluded to in the reference guide:Multispee...

marcie by Associate
  • 1279 Views
  • 2 replies
  • 0 kudos

STM32l052 exti problem

Posted on August 22, 2015 at 20:27Hi. I have three buttons connected to PB12, PB13, PB14. I use the following code:   GPIO_InitStruct.Pin = GPIO_PIN_12 | GPIO_PIN_13| GPIO_PIN_14;   GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING;   GPIO_InitStruct.Pull ...

baev_al by Associate III
  • 1522 Views
  • 6 replies
  • 0 kudos

HAL_UART_Transmit_DMA

Posted on October 21, 2015 at 19:20Hi,I am using STM32F746.It is connected with ST wifi module(SPWF01SC) via UART./* Buffer used for transmission */uint8_t aTxBuffer[] = ''AT+S.SOCKD=8825\r\n'';/* Buffer used for reception */uint8_t aRxBuffer[RXBUFF...

Nandy K by Associate II
  • 957 Views
  • 0 replies
  • 0 kudos

STM32 DFU Bootloader Deleted

Posted on October 21, 2015 at 10:25Hello. I'm using an STBee evaluation board that has STM32103VE.I accidentally overwritten the bootloader using the ULINK2 debugger using Keil.I thought there should be no problem since I have the DFU hex file but a...

TIMx Input Capture Prescaler does not work

Posted on October 21, 2015 at 13:26 I'm experiencing a problem very similar to the post titled ''Design Anomaly with TIMx...'' using the STM32F429i-DISCO Board and IAR Workbench. Despite several related posts, I have not found a solution. My 2-ch...

STemWin libraries

Posted on October 16, 2015 at 10:54I've found that on the ST32F429 DISCO that the library STemWin STemWin522_CM4_OS_GCC.a works and yet the later version STemWin528_CM4_OS_GCC.a does not. Its hangs somewhere after GUI_X_Config(). I have the CRC modu...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.