2023-03-26 3:05 AM
Hi all
I'm using a Nucleo U575 board for reading a GNSS module. I configured the USART2 port with DMA (in circular mode, port 0 as it's peripheral to memory), Request is USART2_RX, Interrupts for USART2 and GPDMA1 are enabled and it works just fine. I'm calling
uint8_t gnss_message[100] = {0};
HAL_UART_Receive_DMA(&huart2, gnss_message, sizeof(gnss_message));just before entering the while-loop in main(). Therefore I'm receiving the NMEA messages of my GNSS module continusously.
To have a constant array I'd like to pause the DMA action during some operation:
HAL_StatusTypeDef hal_return = HAL_OK;
hal_return = HAL_UART_DMAPause(&huart2);
/** some action on gnss_message array **/
hal_return = HAL_UART_DMAResume(&huart2);When debugging the code, hal_return stays HAL_OK all the time. So I assume the HAL_UART_DMAPause/Receive() function is called properly. But for some reason, gnss_message still gets updated with the incoming bytes during /** some action **/
What did I miss? What's the correct way to call HAL_UART_DMAPause() and HAL_UART_DMAResume()?
Thanks in advance
2023-04-03 4:30 AM
I'm still struggling with pausing the UART_DMA process as described above. I can use it without any issue in a clean new project. But when including the functionality to my ThreadX/TouchGFX project, the DMA process doesn't pause.
Is there a incompatibility with ThreadX and HAL_UART_DMA functions? Does anyone know something about it? Or any other reasons why the HAL_UART_DMA_Pause() function may not work properly?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.